Skip to main content
cr_it
Associate
Apr 8, 2016 3:04 PM UTC
Question

STM8 Linker: text size overflow ... just in Release ... not in Debug

Posted on April 08, 2016 at 17:04

Hello everyone!

Currently I'm switching from an Atmel ATTiny to a STM8 microcontroller and so I'm evaluating different IDEs and compilers. I started with a combination of the ST Visual Development and the COSMIC STM8 Compiler (Cosmic CXSTM8 Special Edition 4.4.4). So far, it worked quite nice. I migrated the ATTiny code step by step to the STM environment. I always used both, the Debug builds and Release builds on my target. But at one point, there seems to be a limit to the Release build:

Running Linker

clnk -l''C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Lib''  -o Release\stm8s003.sm8 Release\stm8s003.lkf 

#error clnk Release\stm8s003. segment .text size overflow (164)

 The command: ''clnk -l''C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Lib''  -o Release\stm8s003.sm8 Release\stm8s003.lkf '' has failed, the returned value is: 1

exit code=1.

When I remove code, the number (164) reduces. The Debug build is ok without any problems. Is there any limit to the linker? or does anyone have a hint? 

Thanks!

Chris

    This topic has been closed for replies.

    2 replies

    cr_it
    cr_itAuthor
    Associate
    Apr 8, 2016 4:37 PM UTC
    Posted on April 08, 2016 at 18:37

    Ok, damn, - it was just the code size.

    I switched the optimization to ''minimize code size'' and now it works :)

    ...Also ''split functions into separate sections'' works

    But how can I see how big my code is? Is there a statistic somewhere? - In the programmer window I can just see how big the .s19 files are... and in my case they are always same size.

    luca239955_stm1_st
    Associate
    Sep 8, 2016 1:47 PM UTC
    Posted on September 08, 2016 at 15:47

    the map file created by the linker contains all the information you need about code size and memory usage.

    Regards,

    Luca