Skip to main content
jamesfowkes
Associate
Mar 6, 2011 10:34 PM UTC
Question

STM8 EXTI Clear Interrupt Flag

Posted on March 06, 2011 at 23:34

STM8 EXTI Clear Interrupt Flag

#interrupt #gpio #exti
This topic has been closed for replies.

5 replies

lowpowermcu
Associate III
May 17, 2011 1:12 PM UTC
Posted on May 17, 2011 at 15:12

Hi james,

Which STM8 deice are you using STM8S or STM8L ?

jamesfowkes
Associate
May 17, 2011 1:12 PM UTC
Posted on May 17, 2011 at 15:12

Hi,

I'm using the STM8S (specifically the STM8S105C6).

James

jeff239955_stm1_st
Visitor II
May 17, 2011 1:12 PM UTC
Posted on May 17, 2011 at 15:12

Hi

I have a similar question.  I am using an STM8S105.

My question is when does the STM8 uC clear the EXTI interrupt source?  Most other peripherals have an explicit status bit that has to be explicitly cleared by the interrupt service routine(ISR).  For edge sensitive Dig In interrupts I do not have to do anything and the interrupt source is cleared automatically by the uC.

My specific interest is in what happens when I enable two bits on a dig port to be edge-sensitive interrupts, and both edges occur within a few micro seconds of each other so that the first edge causes the micro to respond to the interrupt and the second edge/interrupt occurs during the ISR before it has returned.  Is the second interrupt internally latched and generates a second call to the ISR immediately the first one ends, or is there a time window where the second edge/interrupt is ignored and is lost unless my ISR explicitly checks for it?

Thanks

spiovan9
Associate III
Oct 6, 2011 9:17 PM UTC
Posted on October 06, 2011 at 23:17

Hi James,

did you eventually got a solution about the question?

I came across the same problem in an application which requires to read an encoder potentiometer which ha 2 channels 90° degree shifted each other.

Thank you

Stefano

Viktor POHORELY
ST Employee
Oct 11, 2011 1:04 PM UTC
Posted on October 11, 2011 at 15:04

For STM8S/A devices, there is no status flag to be cleared.

For STM8L devices, there is a status flag to be cleared.

In both cases, if your application timing does not allow to check status of the external pin in the interrupt, I could only recommend to use different ISR for each separate event.