Skip to main content
fggnrc2
Associate III
Apr 29, 2011 5:56 AM UTC
Question

STM8 core bug

Posted on April 29, 2011 at 07:56

STM8 core bug

    This topic has been closed for replies.

    2 replies

    fggnrc2
    fggnrc2Author
    Associate III
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Robert,

    I thank you for your quick reply and workaround!

    When I discovered this bug, it was a very bad piece of news for me, since I need to trust in my tools when I debug my code.

    I'm also happy that this fault lies in the interplay between STM8 hardware and the debug instrument (and not elsewhere), because now I can suppose again that the root of a fault is only in my code.

    EtaPhi

    Nickname14202_O
    Visitor II
    May 17, 2011 1:12 PM UTC
    Posted on May 17, 2011 at 15:12

    Hello,

    The bug only occurs when hardware stepping in some particular cases.

    If you execute the program without hardware stepping, it works.

    There are two possible workarounds if you want to step:

    - use software stepping (Click on ''Debug Instrument'' then on ''Stepping Mode'' and select ''Don't enter interrupts when stepping into''),

    - set a breakpoint on the instruction which doesn't execute correctly when hardware stepping. It also works if you set a breakpoint close to this instruction.

    RJ