STM32 HAL_SPI_Library on Blue Pill
- 27 replies
- 1815 views
Title edited to note that this relates to a Blue Pill board.
Hello everyone,
I'm starting a learning journey into the STM32 world, specifically studying the HAL library (my past programming experiences didn't rely on ready-made libraries).
Right now (after tinkering with GPIOs, LCD management, etc.) I'm working on the SPI dialogue. I have two STM32F103CBT6A development boards, one configured for "Full Duplex Master" and one for "Full Duplex Slave."
When trying to send 10 static bytes (10, 20, 30, 100) from both the master and slave sides using the "HAL_SPI_TransmitReceive_IT(&hspi1, TX_Buffer, RX_Buffer, 10)" function, I expect the oscilloscope to see the MOSI line equal to the MISO line without any offsets. This happens for a few seconds after resetting the slave (image 1), but then the bytes on the MISO line shift (image 2). Furthermore (I'm viewing the data received from the slave on an LCD) when this problem occurs, the slave also doesn't receive correctly.
After adjusting the codes for 10-byte transmission, I wanted to expand it to 150 bytes.
Thanks in advance to anyone who can point out where I'm going wrong.