Skip to main content
punmack
Associate II
Apr 10, 2013 2:13 PM UTC
Question

STLED316S

Posted on April 10, 2013 at 16:13

STLED316S

I would like some clear instructionsthat inform me how to communicate with the STLED316S.

I have the STEVAL-ICB003V board,viewing the communications on a logic analyzer, and attempting to duplicate the setup does not work.

I am connected to the STLED316S with a uC, can get only DIG1_LED to illuminate.

Is there is someone at ST that knows how to point to a memory location and write control values, please do share?

An example that tells how to set the STB line low while pointing to a memory location + page file would be useful.

Example, write to STLED316S to set number of digits, then set to send series of values to each digit for display.

In addition, I am using 3.3V for the serial communications, I am powering the STLED316S with 5V, and pulling DIN/DOUT up with 3.3V. Is this the proper method?

    This topic has been closed for replies.

    1 reply

    punmack
    punmackAuthor
    Associate II
    Apr 10, 2013 7:42 PM UTC
    Posted on April 10, 2013 at 21:42

    Please see STM32 forum for the conclusion to these struggles with documentation.