STiH418 / H418-HUB: BGA pinout for UART and SPI
Hi everyone,
I’m looking for the BGA pinout of an ST device marked H418-HUB, which I believe is an STiH418.
I found the public data brief (DocID026633) and the Linux device-tree sources, but I’m missing the mapping from the logical PIO signals to the physical BGA balls. Specifically, I’m trying to locate:
-
UART10: PIO3[4] (TX) and PIO3[5] (RX)
-
SPI-FSM: PIO40[0–5]
Does anyone know where to find the package ball assignments and the corresponding I/O voltage specifications? I would also be interested in the full hardware reference manual, particularly the sections covering pin multiplexing, UART and SPI-FSM. If access to the complete manual is restricted, a pinout table or an extract covering these interfaces would already be helpful.
I also found references to the 4kopen B2264 board, which used the same SoC and offered schematics and an ST MicroConnect 2 JTAG connection document. However, the 4kopen project appears to have been abandoned: its former website and documentation resources are no longer accessible.
Are these documents still available elsewhere, or is there a suitable ST support contact for this legacy device?
Thanks!