Skip to main content
Visitor II
Apr 13, 2026 9:41 AM UTC
Question

STHS34PF80 - TPRESENCE value converges to 0 and freezes

Hello,

I'm working on a project to increase the detection range of the STHS34PF80. During my tests with different LPF and Threshold settings, I noticed that TPRESENCE_L often drops to 0 and stops updating entirely.

It feels like the internal algorithm is "absorbing" the signal or the filter is too aggressive.

Does changing LPF settings require a specific reset sequence to prevent this?

Are there known limitations when trying to push the range beyond 2.2m using software parameters?

Any help would be greatly appreciated. Thanks!