Skip to main content
Associate II
April 29, 2024
Question

STEVAL STRKT01

Hi I am a new user, Can any please tell me which software do I need to use for STEVAl STRKT01? My aim is to transmit lora signal and received this signal on spectrum analyzer.

This topic has been closed for replies.

10 replies

Andrew Neil
Super User
April 29, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
April 29, 2024

Yes, I have checked the documents. It does not tell about which software to use to access the device. 

Andrew Neil
Super User
April 29, 2024

Your read the UM2541 User Manual ?

And looked on the 'Software' tab?

AndrewNeil_0-1714402147794.png

 

AndrewNeil_1-1714402287462.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
April 29, 2024

Thank you very much, I will try to use this software. 

Associate II
April 29, 2024

Does it have any hardware driver?

 

Andrew Neil
Super User
April 29, 2024

Read the User Manual UM2487, Getting started with the STM32Cube function pack for IoT tracker node with LoRa® connectivity, GNSS and sensors

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate II
July 11, 2024

Hi Andrew, 

I am trying to change device join parameters using serial communication via Putty. It doesnot get changed

Associate II
July 11, 2024

I have updated my firmware of STEVAL-STRKT01 using st nucleo board. The firmware is a binary file file with location {en.fp-atr-lora\STM32CubeFunctionPack_LORA1_V2.2.0\Projects\STEVAL-STRKT01\Applications\LoRa\Asset_Tracker\Binary\STEVAL_STRKT01_EU868.bin}

I have access the module using putty.

The output in putty is 


ST Microelectronics
LoRa Smart Tracker firmware
APP_VERSION= 01.03.00.00
MAC_VERSION= 04.04.02.00
LoRa IOT tracker app version: 2.2.0
Battery voltage 0.00 V
Battery charge: 0%
Charger status 9
BATTERY_TEMP_FAULT_OR_NOT_PRESENT
Got sensor data: T: 28.15 H: 50.77 P: 1014.20
Accelerometer: X: 25 Y: -61 Z: -976
Got coordinates: 52.764061 N, 1.242864 W, ALT:110.160004
19/11/20 16:00:57 - 0 sats - Fix 0
Battery voltage 0.00 V
Battery charge: 0%
Charger status 9
BATTERY_TEMP_FAULT_OR_NOT_PRESENT

Processing command: ?devicejoinparam

DevEui(FromMcuId) = 32 37 32 38 4C 37 7B 08
Application uses the Over-the-Air activation procedure.
Active keys:
DevEui = 32 37 32 38 4C 37 7B 02
JoinEui = 01 02 03 04 05 06 07 08
AppKey = 5F 06 5A 8B 60 5A 0C 2E 12 3C E1 30 5D 53 28 E4
NwkKey = 5F 06 5A 8B 60 5A 0C 2E 12 3C E1 30 5D 53 28 E4

ADR: N, DATA RATE: DR_4, PUBLIC NETWORK: Y
Command complete

I have registered this on ttn network as well. image attached.

hassanmaree_0-1720722019874.png

 

Associate II
July 17, 2024

Hi Andrew, 

 

My device is working fine now and transmitting data through things network. Could you please tell me how can i change spreading factor of the transmitted signal