Skip to main content
Yaron1
Visitor II
December 29, 2020
Question

STB6100 Tuner cause an arbitration lost in the I2C interface. See additional details.

Hi,

We have the STB6100 Tuner in our products, many of them are in the field.

Lately we have been working on a bug in which the STB6100 cause an arbitration lost in the I2C interface.

It seems that writing some specific values to the registers cause this issue.

For example, it happens when we write to register 0x03 the values 0x21/0x22.

Another issue we see is that when writing 0x01 to the register 0x03, the STB6100 forces the value 0x00 instead.

What might cause this issue?

In addition, is there any additional documentation of the STB6100 as Errata etc.?

Thanks,

Yaron.

This topic has been closed for replies.