Skip to main content
krzysztof239955_st
Associate II
Oct 7, 2009 3:45 AM UTC
Question

Stack size in Cosmic

Posted on October 07, 2009 at 05:45

Stack size in Cosmic

    This topic has been closed for replies.

    3 replies

    krzysztof239955_st
    Associate II
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    Hi,

    I use recursive function qsort.

    How can increase the size of the stack?

    I use Cosmic compiler with Stack Long (modsl0) memory model.

    Regards,

    krzysztof.skoczek

    DJC
    Senior
    Jul 19, 2017 11:58 PM UTC
    Posted on July 19, 2017 at 23:58

    I don't know if it helps your issue, but your question has 'recursive' and 'size of the stack' - and that really helped me a lot thanks!. 

    Im running FreeRTOS on STM32F1 series. 

    I also have a recursive function. Mine has programmed limits on its depth, but it was still causing the HardFault_Handler to execute. 

    I fixed it by increasing the stack size on the FreeRTOS thread. In this case form 128 to 256. 

    osThreadDef(Handle, StartHandler, osPriorityBelowNormal, 0, 256);

    I was able to make the setting the the CubeMx configuration as well. 

    Thanks again!

    luca239955_st
    Associate II
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    Hello,

    there's no need to increase the stack size, as this is not a parameter you can control (at least directly) in your source files or application settings.

    In a typical stm8 application, the stack is initialized at the highest ram address and then grows backwards: if it grows too much, one of the two things below will happen, both leading to unpredictable system behaviour (crash!):

    - the stack will overwrite some other memory area (probably global variables)

    - the stack pointer will wrap around to its original value (hardware limitation)

    Regards,

    Luca (Cosmic)