Skip to main content
Associate II
Sep 5, 2025 1:35 PM UTC
Question

STA540 BTL parallel

Dear technical team

I'm designing a triamped system with the STA540 , in fact it uses two STA540's per unit.

nachus001_0-1757079172338.png

 

 

I've divided the system in one STA amplifying stereo treble and mid, and other STA for bass amplifier, but given that bass channel is not stereo (has the sum of L and R bass, I'd like to know if I may parallell channels 1 || 3 and 2 || 4 for a single bridge amplifier, instead of using only one bridge (1-2 or 3-4)

Can this chip operate with parallell channels? If it can, is it okay to use the channels that I've listed, or there is a better channel pairing?

Best

Ignacio

1 reply

nachus001Author
Associate II
Dec 8, 2025 10:37 PM UTC

Hello

 

Can the STA540 be connected in this way without problems?

Thanks in advance

Ignacio