Skip to main content
siegmund
Associate III
Mar 16, 2005 4:41 AM UTC
Question

ST92F150 with external SRAM 32K: problems

Posted on March 16, 2005 at 05:41

ST92F150 with external SRAM 32K: problems

This topic has been closed for replies.

3 replies

siegmund
siegmundAuthor
Associate III
May 17, 2011 9:36 AM UTC
Posted on May 17, 2011 at 11:36

Hi,

it seems to be a timing-problem with R/W.

in mode=1 (and removing the inverter for AS->ALE) the sram runs perfectly.

unfortunately, we can't switch the design to mode=1, cause on the same data/adressbus there's a graphic-LCD which doesn't run with mode=1.

And: sram should work with mode=0 (as shown in datasheets)! :-W

anybody any hints?

siegmund
siegmundAuthor
Associate III
May 17, 2011 9:36 AM UTC
Posted on May 17, 2011 at 11:36

Hi professionals,

we're using the ST92F150CV1 for about 18months in production (about 1000 pieces). Suddenly we have problems with the external SRAM: it's no more possible to write data in it.

Facts:

CPU-Speed: 12MHz, Core-Speed: 6MHz, DS-strecht: MAX, AS-Strech: MAX

mode control: Mode=0, ETO=off, BSZ=1,

circuit as in ST9-Datasheet V4, page 143, mode=0

ram: div. manufacturers (samsung, issy), 70ns and 55ns

the messured cycle-time is about 1usec (very slow!)

playing with waitstates, different configurations, different rams shows no way to fix the problems.

on some boards reducing waitstates (as/ds) brings success, but not on the others. mode=1 (with rewiring AS to ALE) brings success on one board, but not on the others.

are there any known (but inofficial) timing-probs with the EMI?

(such as the new chapter ''KNOWN LIMITATIONS'' in datasheet V4?

(app notes an1069 + an1076 are well known).

has anybody successfull created a board with such a configuration?

need help!

siegmund
siegmundAuthor
Associate III
May 17, 2011 9:36 AM UTC
Posted on May 17, 2011 at 11:36

hi there,

another facts (problem is still existing):

i attached diagramms of 4 accesses to the sram:

2x write:

- write AD=2, Data=1

- write AD=3, Data=2

2x read

- read AD=2: >> Data=3 (fail!!!)

- read AD=3: >> Data=2 (correct)

why doesnt work the first write?

the naming conventions are for sram, the mode in st9 is mc=0 (oe/ which is ds/ from st9 has one cycle in mc=0).

and, as you can see in the diagramms, all waitstates are activated, so access is slow.

what is wrong in first write-access?

thank you professionals!

siggi