Skip to main content
roberto239955
Associate II
Jun 20, 2003 9:53 AM UTC
Question

ST90T40 CAN communication problem at startup

Posted on June 20, 2003 at 11:53

ST90T40 CAN communication problem at startup

This topic has been closed for replies.

3 replies

roberto239955
Associate II
May 17, 2011 9:33 AM UTC
Posted on May 17, 2011 at 11:33

We have a problem with the interface between the uC ST90T40 and the SJA1000 controller:

- when we switch-on the circuit the first time, the communication between the card and the other equipment through the CAN communications network is right.

- When we switch-off and switch-on the circuit with a time difference below 2 seconds (aprox.), with some micro controllers the CAN communication is right and with other micro controllers the same function isn’t right.

The SJA1000 is a CAN communication controller and the uC is the responsible for configuring the SJA1000.

The SJA1000 is accessed as a memory from uC using P0DR as alternate function:

Do you know if it's something already known?

thanks a lot Fiorenz
labafile
Visitor II
May 17, 2011 9:33 AM UTC
Posted on May 17, 2011 at 11:33

Sir,

Did you ever find a solution to this difficulty? Sounds like something we just encountered?
romain2399
Associate II
May 17, 2011 9:33 AM UTC
Posted on May 17, 2011 at 11:33

The problem description is not enougth detailled: did you analyze the Port0 bus signals and the SJA1000 signals during a failure compare with a good device ?