Skip to main content
johan239955_stm1_stmicro
Associate III
Nov 20, 2002 12:33 PM UTC
Question

ST9 : DIV2 mandatory when using PLL ?

Posted on November 20, 2002 at 13:33

ST9 : DIV2 mandatory when using PLL ?

This topic has been closed for replies.

3 replies

romain2399
Associate II
May 17, 2011 9:32 AM UTC
Posted on May 17, 2011 at 11:32

If you do not use the initial divider-by-2 you may increase your PLL jitter ?

sjo
Associate III
May 17, 2011 9:32 AM UTC
Posted on May 17, 2011 at 11:32

I don't actually see a problem doing this, the DIV2 bit is not used in the 92163 USB devices to obtain the correct internal frequency.

Regards

Spencer Oliver

Anglia
johan239955_stm1_stmicro
Associate III
May 17, 2011 9:32 AM UTC
Posted on May 17, 2011 at 11:32

Based on the datasheet, it looks like the DIV2 (see MODER register) is required when using a crystal :

''Since the input clock to the Clock Multiplier circuit requires a 50% duty cycle for correct PLL operation, the divide by two circuit should be

enabled when a crystal oscillator is used''

However, how can we reach the ST9 maximum clock speed (24MHz) with a standard crystal ?

The easiest solution would have been to clock the micro with a 4Mhz crystal and remove the DIV2 option.

Does anyone have tried to remove the DIV2 bit ?

Did it work with your design ?

Jojo