Skip to main content
marc
Visitor II
March 27, 2014
Question

st8 Discovery gdi-error [40201]: can't access configuration database

Posted on March 27, 2014 at 20:09

Hi,

I'm trying to use the ST Visual Develop with the Cosmic st8 32k compiler.  I install everything and build the project.  That all works fine.  When I try to connect to the Discovery board with the debugger using Swim ST-link, I receive the following error:

Starting debug session...

 

 -> Emulator reset (usb://usb)...

 

  ** Connection error (usb://usb): gdi-error [40201]: can't access configuration database

 

 

 

 -> Failed to connect target.

I have tried uninstalling and re-installing everything including the drivers.  I've tried other target settings.  The only one that works is the simulator.

When I connect the Discovery board, my computer sees it as an external HD.  I get the pop-up window and can look at the links stored on the board.  I'm using Windows 7 64bit.

I should also add that after the above error message a windows 7 pop-up appears saying that gdb7 has stopped working and a red LED glows on the board.

Any help would be appreciated.

Regards,

Marc

#stm8-discovery #i-also-get-same-error-so-please
    This topic has been closed for replies.

    43 replies

    stephenstephen9
    Visitor II
    August 27, 2015
    Posted on August 27, 2015 at 23:05

    Please help me.

    I'm trying to use the STM8S Discovery dev board  and I keep getting errors when I try to use the ST-Link to debug it.

    can't access configuration database.  I have no idea why? or what the config database is?  I've tried installing everything, reinstalling everything.  I've tried two different computers and 4 different boards, and two different ST-links? I'm using windows 8.  Any ideas?

    S C
    ST Employee
    August 28, 2015
    Posted on August 28, 2015 at 14:00

    Hello Stephen,

    Did you try what I explained in the previous post (26 august) ?

    The concerned database is stvd/swim/config/swim_conf.mdb. It requires the DAO-3.5 jet engine to be installed on the system. This is expected to be done by ST Toolset.msi, as explained in previous posts. Perhaps are you facing some other issue: to ensure, please have a look at the file stvd/swim/error.log after the error. If it differs from my previous hypothesis, please post it.

    Best regards
    anamahoot
    Visitor II
    September 21, 2015
    Posted on September 21, 2015 at 11:42

    Dear SC,

    i got similar on windows 10. register DAO with admin right work perfect. 

    thank you and best regards,

    alongkorn

    e2pro
    Visitor II
    September 21, 2015
    Posted on September 21, 2015 at 16:13

    I tried this solution suggested on Windows 10 and works perfectly. Thanks!

    mau100x100
    Visitor II
    September 22, 2015
    Posted on September 22, 2015 at 12:17

    Hello,

    I tried to follow your indication on a Windows 7 system in order to solve the GDI error [40201]: can't access configuration database. Note that Windows system is installed in drive F:

    I tried to run ''ST Toolset.msi'' fron DAO folder, using recovery mode; the installation seems OK. But the error remains.

    The error.log file is attached to this post.

    After unregistered theDAODLL; but when I tried to register again the DLL an error occurred:

    ''The module F:\Program File\Common Files\Microsoft shared\DAO\DAODLL has been loaded but the call to a DllRegisterServer failed. Error code 0x80004005''

    May I try some other way?

    Thank You

    Maurizio

    ________________

    Attachments :

    Error.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzN6&d=%2Fa%2F0X0000000bKe%2FCcsHawjIbnI1lBVlMpDtXSXmoiXjFgAOsMc_rpg9HsU&asPdf=false
    mau100x100
    Visitor II
    September 22, 2015
    Posted on September 22, 2015 at 12:17

    Hello,

    I tried to follow your indication on a Windows 7 system in order to solve the GDI error [40201]: can't access configuration database. Note that Windows system is installed in drive F:

    I tried to run ''ST Toolset.msi'' fron DAO folder, using recovery mode; the installation seems OK. But the error remains.

    The error.log file is attached to this post.

    After unregistered theDAODLL; but when I tried to register again the DLL an error occurred:

    ''The module F:\Program File\Common Files\Microsoft shared\DAO\DAODLL has been loaded but the call to a DllRegisterServer failed. Error code 0x80004005''

    My I try some other way?

    Thank You

    Maurizio

    ________________

    Attachments :

    Error.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzN1&d=%2Fa%2F0X0000000bKf%2Fg4i4mGXhIA64z4DZhIIfiCUx.7g6jNwom5Qpe6ZKelI&asPdf=false
    dtpnilsson
    Associate II
    February 27, 2016
    Posted on February 27, 2016 at 12:36

    Hi,

    I am having the same problem as Maurizio. I've followed everything detailed in this post (including numerous reinstalls) and I still get the gdi-error. When removing the DLL and adding it again, I receive the same error as Maurizio.

    It's a stock installation on C:\ using Windows 8 64 bit.

    dtpnilsson
    Associate II
    March 4, 2016
    Posted on March 04, 2016 at 10:59

    ''DllRegisterServer failed. Error code 0x80004005''

    I solved this by running the command prompt as administrator (I wasn't aware that I didn't do this before), Win-button -> search for command -> right click Command Prompt -> click Run as administrator. DLL now registers and debug works, issue is fixed.

    bala21ece
    Associate
    June 3, 2016
    Posted on June 03, 2016 at 13:39

    SChow
    Associate
    November 13, 2018

    I am getting the below error after flashing the code and when tied to enter debug mode

    ---------------------------

    ST Visual Develop

    ---------------------------

     ** Connection error (usb://usb): gdi-error [40201]: can't access configuration database

    ---------------------------

    OK  

    ---------------------------

    1) I tried this,  ''C:\Program Files (x86)\STMicroelectronics\st_toolset\stvd\dao\ST Toolset.msi'' , Did not work.

    2) Tried this : cmd.exe - run as administrator

    Regsvr32 /u ''C:\Program Files (x86)\Common Files\Microsoft Shared\DAO\DAO350.DLL''

    Regsvr32 ''C:\Program Files (x86)\Common Files\Microsoft Shared\DAO\DAO350.DLL''.

    Did not work.

    :( :( :(