Skip to main content
laurent239955_stm1
Associate
Feb 27, 2006 1:03 PM UTC
Question

ST7Ultralite : Amazingly small ... tremendously useful !

Posted on February 27, 2006 at 14:03

ST7Ultralite : Amazingly small ... tremendously useful !

This topic has been closed for replies.

4 replies

laurent239955_stm1
Associate
Feb 15, 2006 4:19 AM UTC
Posted on February 15, 2006 at 05:19

Hello,

I'm happy to announce you that our new ST7Ultralite is now available.

This is a 8-pin chip working from 2.4v to 5.5v, embedding :

- an internal RC 8MHz oscillator,

- an auto wake-up 33kHz oscillator,

- with low voltage detection capabilities,

- 1k of single voltage Flash programming memory.

- a 12-bit Auto Reload Timer with output capture and PWM,

- a 8-bit Timer with watchdog,

- a 10-bit A/D converter (up to 5 channels),

- 6 I/O lines (5 with High Sink capabilities),

- 5 power saving modes,

- available in DIP8, SO8 and DFN8 packages,

- less than 16 mm² in DFN8.

This is a small micro bursting with features.

You can find all the detailed information by searching for ''ultralite'' in the ''Search ST MCU'' field or by having a look to the official press release :

http://www.st.com/stonline/stappl/press/news/year2006/p1768.htm

Feel free to ask your questions in this forum.

Best regards

Laurent

hazem
Visitor II
Feb 21, 2006 9:31 PM UTC
Posted on February 21, 2006 at 22:31

HI

HOW R U .HOPE FINE . I AM CONCERNED WITH HOW TO INCIRCUIT PROGRAM THE MICRO ST7ULTRALITE WITH THE USB STVD7-INDARTSTX- . THE KIT DOESN'T SUPPORT IT IN ITS DEVICES .SO HOW CAN I PROGRAM IT ?

I TRIED THE ST7FLIE0 CNFIGURATIIONS , IT DOESN'T WORK

SO CAN YOU PLEASE ADVISE ME OF HOW TO PROGRAM THIS AMAZINGLY SMALL BUT TRMENDOUSLY USEFUL MICRO. :D

info45
Associate
Feb 24, 2006 4:38 PM UTC
Posted on February 24, 2006 at 17:38

Hy,

You have forget to say that this ST7ultralite MCUs have the same shape of microchip PIC10xxx ( EEPROM included! ) and freescale MC68HC908QTx!!

By

laurent239955_stm1
Associate
Feb 27, 2006 1:03 PM UTC
Posted on February 27, 2006 at 14:03

Hello,

The IndartSTX will be soon available. I will update this post as soon as i get a date.

BR

Laurent