Skip to main content
huaer2000
Associate III
Sep 28, 2004 8:38 AM UTC
Question

ST7MDT10_EMU3 problem???

Posted on September 28, 2004 at 10:38

ST7MDT10_EMU3 problem???

This topic has been closed for replies.

2 replies

huaer2000
huaer2000Author
Associate III
Sep 28, 2004 2:58 AM UTC
Posted on September 28, 2004 at 04:58

Dear sir,

while I use St7MDT10-EMU3, there is an error messag like this.

** Connection error (usb://usb): gdi-error in hds:[10004]

no Communication with emulated mcu

Could anyone tell me how to solve this problem.

Best Regards,

Mucinterest
juhee
Visitor II
Sep 28, 2004 8:38 AM UTC
Posted on September 28, 2004 at 10:38

There seems to be a connection error, so you can verify the following:

1. If you are using STVD7 3.0, In the Debug Instument Tab, select the Port at which you have connected the emulator. If you are using old version of STVD7, in the emulator settings select the Port correctly.

2. Try changing the Microconnect (If you have an Extra?)

3. Check the Flex-Cable that you are using