Skip to main content
huaer2000
Associate III
October 9, 2004
Question

st7lite0 PWM question?!!

  • October 9, 2004
  • 6 replies
  • 1032 views
Posted on October 09, 2004 at 03:45

st7lite0 PWM question?!!

This topic has been closed for replies.

6 replies

huaer2000
huaer2000Author
Associate III
May 24, 2004
Posted on May 24, 2004 at 07:50

I write a program like below:

CLR PADR

LD A,#$0F

LD PADDR,A

LD A,#$FF

LD PAOR,A

CLR PBDR

LD A,#0 ;#$7

LD PBDDR,A

LD A,#0 ;#$7

LD PBOR,A

LD A,#$0C

LD ATRH,A

LD A,#$0E0

LD ATRL,A ;PWM frequ0K

LD A,#2

LD PWM0CSR,A

LD A,#$10 ;fcpu= 8MHZ

LD ATCSR,A

BSET PWMCR,#0 ;Enable

loop:

LD A,#$0F

LD DUTY_H,A

LD DUTY_L,A

LD A,DUTY_H

LD DCR0H,A

LD A,DUTY_L

LD DCR0L,A

JRA loop

The problem is the PWM output frequency in the oscilliscope is not stable, it change between 9.8K and 4.9K. I don't know why.

could anyone help me to explain it.

Best Regards,

mcuinterest

jatin
Visitor II
May 26, 2004
Posted on May 26, 2004 at 12:54

It is not the normal behavior. Your code seems to be ok. Pls check your cpu clock on MCO pin and internal RC oscillator settings.

huaer2000
huaer2000Author
Associate III
September 20, 2004
Posted on September 20, 2004 at 03:41

I have checked clock the MCO pin and internal RC oscillator settings, there is no problem. what wrong lite0x bug?

mcuinterest
wolfgang2399
Associate III
September 20, 2004
Posted on September 20, 2004 at 06:04

Perhaps the problem occures because you refresh your Duty Cycle Register in a permanently active loop.

Please notice the text below of the datasheet in the chapter of the Autoreload Timer:

Caution: As soon as the DCR0H is written, the

 

compare function is disabled and will start only

 

when the DCR0L value is written. If the DCR0H

 

write occurs just before the compare event, the

 

signal on the PWM output may not be set to a low

 

level. In this case, the DCRx register should be updated

 

just after an OVF event. If the DCR and ATR

 

values are close, then the DCRx register shouldbe

 

updated just before an OVF event, in order not to

 

miss a compare event and to have the right signal

 

applied on the PWM output.

Hope it helps

WoRo
sjo
Associate III
September 20, 2004
Posted on September 20, 2004 at 07:09

In your code you are constantly writing to the DCR0 register, this only has to be done once for setup and then only if you need to change duty cycle.

This could cause a problem as the compare is frozen when the DCR0H is written as mentioned above.

Regards

sjo
huaer2000
huaer2000Author
Associate III
October 9, 2004
Posted on October 09, 2004 at 03:45

Dear sir,

you are right, now I update the duty cyle in the overflow interrupt subroutine

of auto reload timer. but the problem(PWM output wave form is not very stable) still exists in some duty cyle point(8%-12% around). I don't know why

I guess it is because the DCR and ATR are very close. Just like the suggestion in the datasheet, the DCRx register shouldbe

updated just before an OVF event, in order not to

miss a compare event and to have the right signal

applied on the PWM output. But I don't know how to update the DCR value befor OVF envent. can anyone help me!.

Best Regards,

mcuinterest