Skip to main content
roberto239955_st
Associate
December 5, 2003
Question

ST72F324 EMC issues

  • December 5, 2003
  • 3 replies
  • 863 views
Posted on December 05, 2003 at 06:05

ST72F324 EMC issues

This topic has been closed for replies.

3 replies

roberto239955_st
Associate
December 2, 2003
Posted on December 02, 2003 at 11:41

I am running an ST72F324 with an external 16MHz crystal and need this speed for performing complex alogrithms.

The problem is that during EMC testing there are peaks at harmonics of 16MHz which are over the limit, that I'm sure are coming from the ST7.

I am using a 2 layer board with ground plane and close decoupling. Would I benifit using the PLLx2 and a 4MHz crystal to reduce these peaks or are there other things I can do
jatin
Visitor II
December 4, 2003
Posted on December 04, 2003 at 12:52

Could you give me the exact name of the device?

thanks.
roberto239955_st
Associate
December 5, 2003
Posted on December 05, 2003 at 06:05

The part no of the device is

ST72F324K2T6