Skip to main content
gavin1
Associate II
Apr 24, 2007 3:50 PM UTC
Question

ST7 Programmer - Illegal System DLL relocation

Posted on April 24, 2007 at 17:50

ST7 Programmer - Illegal System DLL relocation

This topic has been closed for replies.

3 replies

gavin1
gavin1Author
Associate II
Apr 12, 2007 10:29 AM UTC
Posted on April 12, 2007 at 12:29

I noticed today after recently changeing over from the IDEA (Cosmic IDE) to ST7 Visual Develop. I am getting an error when running the ST7 programmer:

stvp.exe - Illegal System DLL Relocation

The system DLL user32.dll was relocated in memory. The application will not run properly. The relocation occurred because the DLL C:\Windows\system32\HHCTRL.OCX occupied an address range reserved for Windows system DLLs. The vendor supplying the DLL should be contacted for a new DLL.

I'm not sure if this is related to HHCTRL.OCX but was wondering if anyone else has had the same problem?

laurent239955_stm1
Associate
Apr 12, 2007 10:44 AM UTC
Posted on April 12, 2007 at 12:44

Hi,

This has been yet reported and it is related to a Microsoft update :

The problem doesn't come from STVP7 but from the windows update

Microsoft has fixed the problem:

==>

http://support.microsoft.com/kb/935448/en-us

Best regards

Laurent

dpeter
Associate II
Apr 24, 2007 3:50 PM UTC
Posted on April 24, 2007 at 17:50

Thanks for the information, I was starting to panic. MS wasn't much help until you displayed the link.

Thanks

Dave P :D