Skip to main content
nirn
Associate II
November 6, 2003
Question

ST7 Maximum Baud Rate ?

  • November 6, 2003
  • 8 replies
  • 1456 views
Posted on November 06, 2003 at 13:45

ST7 Maximum Baud Rate ?

This topic has been closed for replies.

8 replies

nirn
nirnAuthor
Associate II
November 5, 2003
Posted on November 05, 2003 at 04:42

Hi,

I'm looking for a ST7 chip with the maximum Baud rate (SCI) For RS232 communication - So far I saw only 500k - does any one know on any other chip with faster UART ?

Thanks
itsmejatinus
Associate III
November 6, 2003
Posted on November 06, 2003 at 04:30

What i know is Maximum baud rate possible is 38.4 Kbps. Where have you found 500k?

nirn
nirnAuthor
Associate II
November 6, 2003
Posted on November 06, 2003 at 05:43

Well....I'm working with the ST72321 and according to the Data Sheet you can reach 500k baud rate in the SCI.

sjo
Associate III
November 6, 2003
Posted on November 06, 2003 at 05:47

500k is available will the following config @ 8MHz cpu:

TR & RR=1, PR=1

Regards

sjo
shermantec
Associate III
November 6, 2003
Posted on November 06, 2003 at 12:16

Hello

Can i get 1M or even more ?

Latino

sjo
Associate III
November 6, 2003
Posted on November 06, 2003 at 12:17

I'm afraid as per the datasheet - 500k max for the sci

Regards

sjo
nirn
nirnAuthor
Associate II
November 6, 2003
Posted on November 06, 2003 at 12:23

I've checked - According to the Data Sheet in my hands - using 16MHz osc can give you SCI with a 1M maximum.

Take a look on the Formula:

Fcpu

Tx = ------

16 * ETPR*(PR*TR)

Fcpu

Rx =--------

16 * ERPR*(PR*RR)

So if ERPR=PR=RR = 1 and Fcpu=16Mhz => you can get 1M Baud Rate !!!!

BUT !!! I've checked and tried it --- and you can't !!!! the Max is 500K

[ This message was edited by: TeaMaker on 06-11-2003 16:54 ]
sjo
Associate III
November 6, 2003
Posted on November 06, 2003 at 13:45

Remember the maximum fcpu for the st7 is 8MHz not 16MHz.

Regards

sjo