Skip to main content
terryhao
Associate III
September 8, 2003
Question

st7 compile error

  • September 8, 2003
  • 5 replies
  • 1043 views
Posted on September 08, 2003 at 09:04

st7 compile error

This topic has been closed for replies.

5 replies

terryhao
terryhaoAuthor
Associate III
September 4, 2003
Posted on September 04, 2003 at 07:58

Recently I meet a problem while I use ST7 assembly to

compile my program. the error message is ''could not

find the ''st7.tab'. I have checked and found the file

st7.tab is in the folder. In addition the path is also setup.

So, I don't know why. coudl anyone help me explain it?

Best Regards,

terry
sjo
Associate III
September 5, 2003
Posted on September 05, 2003 at 07:14

The only thing I can suggest is to check METAI variable is defined with the correct path to the assembler (usually C:\Program Files\STM\st7toolchain\asm) and to double check st7/ or ST7/ is defines at the top of each source file (check there are no spaces etc)

Have you tried reinstalling the assembler ?

Hope this helps

sjo
terryhao
terryhaoAuthor
Associate III
September 5, 2003
Posted on September 05, 2003 at 07:36

Thanks first.

I have reinstall the software. But there is no use. If I put

''C:\Program Files\STM\st7toolchain\asm\st7/'' in the .asm file. the

7lite0.asm and constant .asm can pass the compile process. But

the ex6c.asm can not pass and the error message is as follows:

'':\Exercise\Result\broteck>asm ex6c.asm -li

Couldn't open source file: No such file or directory''

but the file is exist in the directory

I don't know why. In addition do you receive my question about

free st7 program?

Best Regards,

Terry

sjo
Associate III
September 5, 2003
Posted on September 05, 2003 at 08:30

The only other suggestion is to attach your code.

Regards

sjo
shreya
Visitor II
September 8, 2003
Posted on September 08, 2003 at 09:04

Hello,

I am attaching a copy of the example. It is compiling correctly for me.

________________

Attachments :

ex6c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I09j&d=%2Fa%2F0X0000000bUX%2FwkDqzyWLk.WLnEkjswJbfVvIYmYZ8NbFby.sP9bLZI0&asPdf=false