Skip to main content
roland2399
Associate
Jun 16, 2006 8:22 AM UTC
Question

ST10Flasher max CPU

Posted on June 16, 2006 at 10:22

ST10Flasher max CPU

This topic has been closed for replies.

2 replies

roland2399
Associate
Jun 16, 2006 6:20 AM UTC
Posted on June 16, 2006 at 08:20

Hi,

what's the maximum CPU frequency the ST10Flasher can handle?

If the ST10flasher refuses to work for frequencies higher than 40 Mhz on the target, is it that we have a problem in our target board or is that limit built into the ST10Flasher ?

Kind regards

najoua
Associate
Jun 16, 2006 8:22 AM UTC
Posted on June 16, 2006 at 10:22

Hello,

The ST10Flasher can be used without problems at frequencies above 40Mhz.

I suppose that you are using the ST10Flasher to program the ST10F276 internal Flash given that it is the only ST10 Family having as Fcpu max 64Mhz.

Could you please confirm that you are using the ST10F276?

If yes, please, make sure that you are using the last ST10F276 version because the old ST10F276 versions have problems at frequencies above 40MHz.

Regards,

Najoua.