Skip to main content
urik
Associate III
Mar 7, 2006 7:45 AM UTC
Question

ST10F276 Read setup time

Posted on March 07, 2006 at 08:45

ST10F276 Read setup time

This topic has been closed for replies.

5 replies

urik
urikAuthor
Associate III
Mar 7, 2006 2:15 AM UTC
Posted on March 07, 2006 at 03:15

Hello,

what is the data set-up time when i use the demuxed bus, with no read delay?

is that T15 ?

if so does it means that the setup time is 18.5 ns? or if i use a 55 ns SRAM i can latch the data after 55ns and not 55 + 18.5 ns?

thanks,

Uri.

najoua
Associate
Mar 7, 2006 4:12 AM UTC
Posted on March 07, 2006 at 05:12

Hello,

Yes, the data set-up time when using the demuxed bus, with no read delay is t15.

If Fcpu = 40Mhz: t15= 18.5 + tc (ns) & tc = 2TCL x (15 - MCTC) ; with 15 - MCTC is the number of wait states.

--> so t15 value is Fcpu and external memory access time dependent.

Let's take an example:

ST10 Frequency is 40 Mhz. Thus the CPU cycle is 25ns. Assuming that the memory has an access time of 55ns= 25ns + 30ns, in order to access this memory, 2 wait states should be

inserted in the EBC cycle.

In this case:

t15= 18.5 + 25x2 = 68.5ns.

If CPU Clock is Variable (from 1 to 64MHz):

t15 = 3TCL – 19 + tC.

I hope i was clear.

Regards,

Najoua.

[ This message was edited by: Najoua on 07-03-2006 09:44 ]

urik
urikAuthor
Associate III
Mar 7, 2006 4:51 AM UTC
Posted on March 07, 2006 at 05:51

Najoua Hi,

you were not so clear , does the T15 <= 18.5 + Ext mem acc time

or T15 <= Ext mem acc time - 18.5 ?

if i am not worng for 55ns i need 3 wait states?

can you please clear this point?

thanks,

Uri.

najoua
Associate
Mar 7, 2006 6:04 AM UTC
Posted on March 07, 2006 at 07:04

Hi Ukatry,

I will clarify,

t15 <= 18.5 + tc;

tc = 2TCL x (15 - MCTC) which depends on Fcpu and the number of wait states in order to be able to acceed the memory.

For a memory having an access time of 55ns:

- at least 2 wait states must be added when Fcpu = 40Mhz because: 55 ns = 25 ns + 30 ns and 30/25 = 1.2 so 2 waitstates are needed.

- at least 3 wait states must be added when Fcpu = 64 Mhz

because: 55 ns = 15.6 ns + 39.4 ns and 39.4/15.6 = 2.5 so 3 waitstates are needed.

I hope it is clear now.

Regards,

Najoua.

[ This message was edited by: Najoua on 07-03-2006 11:39 ]

urik
urikAuthor
Associate III
Mar 7, 2006 7:45 AM UTC
Posted on March 07, 2006 at 08:45

now it is clear , thank you very much.