Skip to main content
rana
Associate III
Nov 20, 2006 4:04 AM UTC
Question

ST10F276 : Program access protected I-Flash from the I-Flash

Posted on November 20, 2006 at 05:04

ST10F276 : Program access protected I-Flash from the I-Flash

This topic has been closed for replies.

4 replies

rana
ranaAuthor
Associate III
Nov 16, 2006 10:55 AM UTC
Posted on November 16, 2006 at 11:55

ST10F276:

I'm going to protect my I-Flash to access.

But...

Will a code running in [B0F0 -> B0F3] able to program [B0F4 -> B3F1]?

Please note:

- The code will program its own BANK but other flash.

- The code must be ran from the I-Flash, due to access protection.

Thanks

Ran

najoua
Associate
Nov 17, 2006 4:13 AM UTC
Posted on November 17, 2006 at 05:13

Hello Ran,

Read/While/Write operation in the same flash bank is not allowed: it is not possible to execute code located in [B0F0 -> B0F3] to program [B0F4 -> B3F1]. In fact, this code must be executed from a bank different from the banks to be programmed. So, Bank1, Bank2 and Bank3 can be programmed without problem but it is not possible to program the remaining Bank0 sectors [B0F4 -> B0F9].

Could you please clarify the statement 'The code will program its own BANK but other flash.'?

----------------

Regards,

Najoua.

[ This message was edited by: Najoua on 17-11-2006 09:50 ]

rana
ranaAuthor
Associate III
Nov 19, 2006 2:37 AM UTC
Posted on November 19, 2006 at 03:37

Same Bank other Flash:

Same Bank = B0

other Flash = F1/F2

B0F1 and B0F2 are the same Bank other Flash...

najoua
Associate
Nov 20, 2006 4:04 AM UTC
Posted on November 20, 2006 at 05:04

Hello Ran,

If I had understood, you want to program [B0F4..B3F1] of FLASH2 which is access protected using a code located in [B0F0->B0F3] of another flash FLASH1.

Could you please confirm?

If this is the case, could you please tell me where the Temporary Access Unprotection routine is located? This routine must already have been located and executed from the protected flash, I mean FLASH2.

Regards,

Najoua.

[ This message was edited by: Najoua on 20-11-2006 09:40 ]