Skip to main content
Associate
August 29, 2023
Question

ST Visual Develop IDE command line compile

Dear ST-Team, 

I am working on a STM8 MCU with the STVD. 
I want to compile my project in the Microsoft cmd line with a pipeline such as . cmd.exe /c "C:\Program Files (x86)\STMicroelectronics\st_toolset\stvd\stvdebug.exe" 

I haven't found any information in the Documentation. Furthermore, there are no help options such as -h, --h, -help and --help  in this program. 

STVD.PNG

 
Are there some documents I can use to write the correct commands to compile the code with the STVD successfully?

Many thanks in advance

Best Regards 
Stefan

    This topic has been closed for replies.

    3 replies

    AA1
    Senior III
    August 29, 2023

    STVD doesn't include the compiler. Read this: Developing and debugging your STM8S-DISCOVERY application code. The recommended compiler is from COSMIC.

    SteZel123Author
    Associate
    August 30, 2023

    Thanks for your quick response. 

    I am using the Cosmic compiler already.  
    I want to use the CMD line. Is there a Possibillity that I can use the CMD with a pipeline for compiling. 
    I have found another documentation from an other manufacturer: Create and Build Projects Using Command Line (ti.com). 
    Is this also with STDV possible? e.g.: cmd.exe /c "C:\Program Files (x86)\STMicroelectronics\st_toolset\stvd\stvdebug.exe  <workspace>  <file location>  <build Parameters>"

    AA1
    Senior III
    August 30, 2023

    I don't know if you can compile from command line using STVD. Probably no. But you can ignore STVD and use the compiler and the linker directly. See Cosmic manual.