Skip to main content
smitt
Associate II
Feb 9, 2005 8:09 AM UTC
Question

ST NAND flash source code help

Posted on February 09, 2005 at 09:09

ST NAND flash source code help

This topic has been closed for replies.

1 reply

smitt
smittAuthor
Associate II
Feb 9, 2005 8:09 AM UTC
Posted on February 09, 2005 at 09:09

Hi.

Im develomping an MP3 player using the source code from ST´s NAND flash memory example. I was actualy rather amased over how much code was needed for a memory stick.

My problem is that I need to add a function to the source code. I have understod that I should call my own functions from the appli.c file. But there is no help file / app. note for this source code, therefore Im having truble understanding it. I need to get a mp3 file from the nand flash but doesnt understand which function I should call on from the MAL(?) library.

I also need some kind of get filelist function that returns directories and filenames stored in the nand memory.

I would appreciate any help. Or links to dokuments and Appnotes clarifying this.

Best regards

Fredrik