Skip to main content
lgiordano2
Associate III
Jan 4, 2006 2:28 PM UTC
Question

ST Library & CrossStudio

Posted on January 04, 2006 at 15:28

ST Library & CrossStudio

This topic has been closed for replies.

4 replies

lgiordano2
Associate III
Jan 2, 2006 3:03 PM UTC
Posted on January 02, 2006 at 16:03

Hi, I am using CrossStudio with a STR711F evaluation board from Olimex. I can't make interrupts work (using ST Library), I think my startup code is wrong. Is there a Start Up Code ready to use with CrossStudio?

Thanks in advance...

Regards,

lgiordano2
Associate III
Jan 3, 2006 10:13 AM UTC
Posted on January 03, 2006 at 11:13

Hey thanks, I am going to test it right now. I am very new to ARM programming, so I hope I can make it work. If not, I will post a new message for help.

Regards,

Leo

lgiordano2
Associate III
Jan 4, 2006 7:16 AM UTC
Posted on January 04, 2006 at 08:16

Hi,

I have some confusion here. When I created a project, CrossStudio generated a startup file. However, it doesn't init EIC or interrupt vectors, which I think is user dependant to do it or not, and the way to do it. My first test was to replace the startup file with the one you provide, but it hanged. Moreover, I couldn't programm the board anymore until some resets and RAM/Flash mode switches and retries.

I attach the startup file I am using, which has a #if .. #else .. #endif to switch between the CrossStudio and yours start up file.

Please look at it and tell me if you find something rare.

Best wishes form Argentina,

Leo

________________

Attachments :

STR71x_Startup.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Hu&d=%2Fa%2F0X0000000bmE%2FGuf4STihpTovP88Bph10KowGtxxfkpQvEvHrGclnTw8&asPdf=false
lgiordano2
Associate III
Jan 4, 2006 2:28 PM UTC
Posted on January 04, 2006 at 15:28

Hi,

I got the attached file from Rowley. It is the complete ST Library ready to use with CrossStudio.

Regards,

Leo

________________

Attachments :

STR71xLibrary_V3_20050608_crossworks.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Nh&d=%2Fa%2F0X0000000bmD%2FFQ76GocEhmZDIKidxR7s.xbw4DxOC1qsGBpHDKdXnqQ&asPdf=false