Skip to main content
mtraman
Associate III
Mar 26, 2007 6:49 AM UTC
Question

SSP NSS bug: Data loops back

Posted on March 26, 2007 at 08:49

SSP NSS bug: Data loops back

This topic has been closed for replies.

3 replies

amira1
Associate
May 17, 2011 7:40 AM UTC
Posted on May 17, 2011 at 09:40

Hi tvikram,

I didn't test your code but as I see:

-In TI mode you can't program CPHA and CPOL bits since bit phase and polarity are applicable to Motorola SPI format only.

-To enable or disable loop back mode, use SSP_LoopBackMode()function and not SSP_LoopBackConfig().

Please find attached an SSP loop back mode example.

I hope this will help you.

Best regards

mirou

mtraman
mtramanAuthor
Associate III
May 17, 2011 7:40 AM UTC
Posted on May 17, 2011 at 09:40

Hi

has anyone solved the loop back problem in SSP?

when the ssp is used in the master mode and data is transmitted on the mosi pin and received on miso pin. transmitted data is correct but the received data is just the copy of transmitted data.

The nss pin is directly connected to the LRC (left right clock) of codec without any pull up resistor. when data that comes on the miso pin is seen in an oscilloscope it is not the transmitted data. the loop back happens inside the microcontroller.

Connecting the nss pin to vcc is not an option for me as the ssp is configured in SSI mode to communicate with a codec.

the code is as follow:

void SSPCodec_Init(void)

{

SSP_InitTypeDef SSP_InitStructure;

// SSP1 configuration

SSP_DeInit(SSP1);

SSP_InitStructure.SSP_FrameFormat = SSP_FrameFormat_TI;

SSP_InitStructure.SSP_Mode = SSP_Mode_Master;

SSP_InitStructure.SSP_CPOL = SSP_CPOL_High;

SSP_InitStructure.SSP_CPHA = SSP_CPHA_1Edge;

SSP_InitStructure.SSP_DataSize = SSP_DataSize_8b;

SSP_InitStructure.SSP_ClockRate = 0; //5- for slave; 0-for master

SSP_InitStructure.SSP_ClockPrescaler = 24;

SSP_Init(SSP1, &SSP_InitStructure);

// Disable the Loop back mode for the SSP1 peripheral

SSP_LoopBackConfig(SSP1, DISABLE);

// SSP1 enable

SSP_Cmd(SSP1, ENABLE);

}

int main(void)

{

u8 cnt=0;

.........

while(1)

{

if(send_ready==1)//wait for 1/48kHz duration, flag is set in tim2 ISR

{

send_ready=0; //reset flag

SSP_SendData(SSP1, sin_data[cnt]);

//wait to receive data

while(SSP_GetFlagStatus(SSP1, SSP_FLAG_RxFifoNotEmpty) == RESET);

mic_data[cnt] = SSP_ReceiveData(SSP1); //Receive the output of mic

cnt++;

if (cnt == NbrOfSamples)

{

cnt = 0;

}

}

}

}

Please, help me out.

Thanks in advance,

vik

mtraman
mtramanAuthor
Associate III
May 17, 2011 7:40 AM UTC
Posted on May 17, 2011 at 09:40

thank u for the reply

i got the solution

it has been posted in the thread - spi slave to master