Skip to main content
neil2399
Associate III
Jun 5, 2006 11:25 AM UTC
Question

SSC clock.

Posted on June 05, 2006 at 13:25

SSC clock.

This topic has been closed for replies.

2 replies

neil2399
neil2399Author
Associate III
Jun 5, 2006 11:03 AM UTC
Posted on June 05, 2006 at 13:03

Hi guys.

I'm interfacing a ST10F269 with a serial flash memory via SPI, and want to know if there is a way I can keep the clock going without transmitting anything. The reason I want to do this, is because to receive data from the flash memory, I need the clock running (duh), but I don't really want to keep on interrupting into a transmit function the whole time.

I hope I've explained myself clearly.

Thanks

Neil

najoua
Associate
Jun 5, 2006 11:25 AM UTC
Posted on June 05, 2006 at 13:25

Hello Vannezil,

It is not possible to keep clock running without transmitting (receive only).

In fact, transmission and reception of serial data is synchronized and takes place at the same time, so the same number of transmitted bit is also received. Furthermore, the clock is generated only when transmission is triggered.

Regards,

Najoua.