Skip to main content
bob2399
Associate II
Jan 14, 2008 12:39 PM UTC
Question

SPI SSN pin

Posted on January 14, 2008 at 13:39

SPI SSN pin

This topic has been closed for replies.

2 replies

bob2399
bob2399Author
Associate II
Jan 7, 2008 3:52 PM UTC
Posted on January 07, 2008 at 16:52

hello everyone! i am currently looking into using the SPI port on the STR712FR2T6 part. i noticed that the SSN pin is always show as pulled HIGH when the uC is the Master. am i to assume that this SSN pin cannot be used as a PORT0 output pin? It cannot be used as the chip select to an SPI EEPROM? so its wasted during Master mode? thanks for any info.

Bob Zeranski

christophe239955_st
Visitor II
Jan 14, 2008 12:39 PM UTC
Posted on January 14, 2008 at 13:39

The SS on the master must be deasserted high :o You have to use another GPIO pin drive the EEPROM chip select line .

Chris.