Skip to main content
hnrymao
Associate
Mar 2, 2009 3:45 AM UTC
Question

SPI Slave to Master

Posted on March 02, 2009 at 04:45

SPI Slave to Master

This topic has been closed for replies.

17 replies

truf9
Associate III
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi,

I use the Keil Starter Kit with the Keil MCB-STR9-Board.

I have the same Problem with the example for the ST-Library, but I did not receive correct data in SPI1.

I tried to set the SPI-Data-In from the master to high or low, but I never get the data 0x00 or 0xFF in the receive-buffer in the Master. I allways have the loopback data from the SPI0-Transmitter.

The Control register 1 from SPI0 is set to 0x0002, so the loopback function is not enabled.

I tried the SPI0 on Port 2 and 5. It's the same.

Regards,

T Ruf

hnrymao
hnrymaoAuthor
Associate
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi,

I use IAR start kits STR912-SK to test the SSP-debug in the examples.eww

workspace which is in ...\ARM\examples\ST\STR91x\STR91xlibrary\examples\directory.

I made a cable to connect the SPI0 connector( Master )and UXT connector( Slave).

When the SPI0( Master ) sends data to SPI1 ( slave), SPI1 can receive the correct data.

When the SPI1 send data to SPI0, the data SPI0 received is not correct. The difference is the slave only can send out data after the master( SPI0 ) send a dummy bit to generate the clock.The data SPI0( Master) received is just the SPI0 send out.

I use scope to monitor the signal SPI1( slave) send out,it's correct,but the contents of SSP0_DR is not correct.

I disconnect the wire between SSP0_MISO(P5.6) and SSP1_MISO(P3.5), the SPI0 can still receive the data which is SPI0 send out.

Following is part of the code.

while(Tx_Idx

{

SSP_SendData(SSP0, SSP0_Buffer_Tx[Tx_Idx++]);

while(SSP_GetFlagStatus(SSP1, SSP_FLAG_RxFifoNotEmpty)==RESET);

SSP1_Buffer_Rx[Rx_Idx++] = SSP_ReceiveData(SSP1);

}

/* Check the received data with the send ones */

TransferStatus1 = Buffercmp(SSP0_Buffer_Tx, SSP1_Buffer_Rx, 32);

/* TransferStatus = PASSED, if the data transmitted from SSP0 and

received by SSP1 are the same */

/* TransferStatus = FAILED, if the data transmitted from SSP0 and

received by SSP1 are different */

/* Clear SSP0 receive Fifo */

for(k=0; k

/* Reset counters */

Tx_Idx=Rx_Idx=0;

/* Slave to master transfer procedure */

while(Tx_Idx

{

SSP_SendData(SSP1, SSP1_Buffer_Tx[Tx_Idx]);

/* send a dummy bit to generate the clock */

SSP_SendData(SSP0, SSP0_Buffer_Tx[Tx_Idx++]);

while(SSP_GetFlagStatus(SSP0, SSP_FLAG_RxFifoNotEmpty)==RESET);

SSP0_Buffer_Rx[Rx_Idx++] = SSP_ReceiveData(SSP0);

}

Anyone has the same problem?

Cheers

truf9
Associate III
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi,

I have connected the SPI the Pin SSP0_NSS directly to VCC. Now i got the right data on MISO and in the receive Fifo. Thanks for the reply.

But I did not understand that i have to connect an Output to VCC.

I want to use the Pin SSP0_NSS as chipselect for an external SPI-Slave in Motorola SPI frame format.

I want to use the SPI-Bus as described in the reference manual of STR91xF at Figure 65.

I want to work with MISO MOSI SCK and NSS to communicate with an external device.

Thanks

stefano239955_stm1_stmicro
Associate III
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi,

I have an IAR starter kit,

I test the SPI sample code and the program works

Did you check if the jumper are connected in the right position.

For default P3x are connected to the leds.

Are you working with 4 lines MISO MOSI SCK and NSS?

hnrymao
hnrymaoAuthor
Associate
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi Stevejamal,

The problem has been solved.The reason is the PIN P57/SSP0_NSS is connected to VCC via a Resistor( R118 10K in STR912-SK EVAL Board ). If this pin tired to VCC directly, it works, otherwise you will see a negative pulse on the pin P57/SSP0_NSS starting before SCLK. The master loopback the sending out data to receiving FIFO automatically.

Thanks,

amira1
Associate
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi lakata,

Concerning the NSS master, it must be pulled up and not to be driven high. However, if you are using the STR9 library example, you have to configure GPIO 2 and GPIO 3 as follow:

GPIO_DeInit(GPIO2);

/*Gonfigure SSP0_CLK, SSP0_MOSI, SSP0_nSS pins */

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Disable;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2 ;

GPIO_Init (GPIO2, &GPIO_InitStructure);

GPIO_DeInit(GPIO3);

/*Gonfigure SSP1_MISO pin */

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Disable;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2 ;

GPIO_Init (GPIO3, &GPIO_InitStructure);

with best regards,

mirou

mark9
Associate III
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

I just discovered this ''feature'' yesterday. Is there a reason why NSS has to be driven high? Is this really something that should be in the Errata? It is a waste of a pin!

gilbert1
Visitor II
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi,

got the same problem, when I use NSS to chipselect the SPI AD Converter I use there is just the send data in my receive buffer.

Now I tied NSS to Vcc like described in this thread and it works, but I have to generate the CS in software as it is needed by this AD Converter to work.

Looking at the NSS output with a scope and looking at a very nice generated CS signal I still think there is a way to use it. Anybody knows how?

thanks

Gilbert

my port init:

GPIO_DeInit(GPIO3);

/*Gonfigure SSP1_CLK, SSP1_MOSI, SSP1_nSS pins */

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_6 | GPIO_Pin_7;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2;

GPIO_Init (GPIO3, &GPIO_InitStructure);

/*Gonfigure SSP1_MISO pin GPIO3.5*/

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable;

GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1;

GPIO_Init (GPIO3, &GPIO_InitStructure);

cfortier
Associate II
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Hi guys,

I've manage to establish a SPI connection with an external SPI-Slave in Motorola SPI frame format on SSP0. Here are my GPIO setting.

GPIO_DeInit(GPIO2);

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Disable;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2 ;

GPIO_Init (GPIO2, &GPIO_InitStructure);

GPIO_DeInit(GPIO3);

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Enable;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt1;

GPIO_Init (GPIO3, &GPIO_InitStructure);

My SSP0_nSS is connected to Vcc with a 10K pull-up resistor.

TRuf, it's working as described in the reference manual of STR91xF at Figure 65.

Hope that could help someone.

Cofor

mark9
Associate III
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

I meant ''driven high externally'' ie connected to VCC. I configured nSS to be an input, and it worked properly for me. I'm just wondering why this pin has to be wasted (it does nothing). Our design ran out of pins...