Skip to main content
scanlon
Associate II
Jun 3, 2005 1:24 PM UTC
Question

SPI operation

Posted on June 03, 2005 at 15:24

SPI operation

This topic has been closed for replies.

2 replies

scanlon
scanlonAuthor
Associate II
Jun 3, 2005 11:47 AM UTC
Posted on June 03, 2005 at 13:47

Hi Everyone.

We are about to switch to STR71 product and I would need a bit of info on the SPI ports. I need to send and receive 32bit words into the STR711 as a SPI slave. Is this possible with the BSPI module? I want to load a 32bit word into the SPI with one long //ss cycle. From what I read, it *looks* like if I clock 32bits into the SPI port, the data will automatically be placed into the next 4 bytes of the buffer.

Does anyone have any thoughts or experience with this? Or maybe details of the specific SPI core that is used?

Thanks in advance,

Ian

scanlon
scanlonAuthor
Associate II
Jun 3, 2005 1:24 PM UTC
Posted on June 03, 2005 at 15:24

Hi RISC,

Thank you for response.

When the spi is slave mode, is a //ss edge required to start and stop transmission?

I don't think I understand the operation of the buffer feature. If I have 4 bytes(to send) in the SPI buffer, what are the requirements to clock that data out? Is a //ss signal required to frame the data into 8 or 16 bits? What I want is to use the //ss signal as a 'gate' to shift 32 bits into 4 bytes in the buffer.

Thanks again