Skip to main content
Philipp Krause
Senior II
Feb 16, 2020 8:57 AM UTC
Question

sourceforge.net

Dear SDCC users,

On the 30th of January SDCC 4.0.0 has been released.

As always it has been put online in the SourceForge File section.

https://sourceforge.net/projects/sdcc/files/

There have been various improvements, both features and bug fixes since

SDCC 3.9.0. The full ChangeLog is at:

https://sourceforge.net/p/sdcc/code/HEAD/tree/tags/sdcc-4.0.0/sdcc/ChangeLog

The following is a list of particularly noteworthy new features.

* The pdk15 backend now passes the regression tests (both with and without --stack-auto), and is thus considered stable.

* New in-development pdk13 backend for Padauk µC with 13-bit wide program memory.

* C2X memccpy(), strdup(), strndup().

* Better tail call optimization.

* Many fixes in the pic14 backend.

* C2X u8 character constants.

* C2X bool, static_assert, alignof, alignas.

* C2X attributes on statements.

* C2X attribute declarations.

* Support for extended ASCII characters in sdas, sdld

* Compiler support for UCNs and non-ASCII utf8 in identifiers

While there is no STM8-specific improvement in the above list, the statistics show show substantial improvements,e.g code size in Coremark: https://sourceforge.net/p/sdcc/code/HEAD/tree/trunk/sdcc-extra/historygraphs/coremark-stm8-size.svg

When I find time, I'll do an update of the STM8 compiler comparison (http://www.colecovision.eu/stm8/compilers.shtml), which currently still reflects the state of SSTM8 C compilers in early 2018.

    This topic has been closed for replies.