Skip to main content
This topic has been closed for replies.

2 replies

joseph2399
Associate II
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

PCON register is NOT bit addressable, only registers reside on addresses x0 and x8 are bit addressable. Although some compilers can use macros to do the bit manipulation; Keil complier does not support it. You need to OR in the bit you want to set or reset.

kobihaun
kobihaunAuthor
Associate II
May 17, 2011 9:53 AM UTC
Posted on May 17, 2011 at 11:53

Hi Every Body

The SMOD bit at UPSD.H is disabled.

When I enable it, the compiler shouts error ''PCON invalid base address''.

How can I enable the SMOD bit in the UPSD.H file?.

Thank you all.

Kobi