Skip to main content
seenivasen
Associate
Mar 29, 2011 1:42 PM UTC
Question

SM8S105 Flash Image(please help urgent)

Posted on March 29, 2011 at 15:42

Hi

I am designing my code using the STM8S Discovery.

When using the Cosmic compiler i get the following files generated after compiling(no debug).

stvd_project_dtd416.elf       (29KB)

stvd_project_dtd416.lkf       (3KB)

stvd_project_dtd416.s19     (27KB)

stvd_project_dtd416.sm8    (31KB)

Which of the above images is actually written to flash. I am implementing a ICP using SWIM which will write the actual image directly to flash program memory so i need to know which image to write.

Need help urgently.

Thanks 

    This topic has been closed for replies.

    2 replies

    brazov22
    Associate III
    Mar 29, 2011 2:33 PM UTC
    Posted on March 29, 2011 at 16:33

    .s19 is memory format in Motorola standard:

    http://en.wikipedia.org/wiki/S19_(file_format)

    http://en.wikipedia.org/wiki/S19_(file_format)

    you can use that.

    brazov2

    seenivasen
    Associate
    Mar 30, 2011 7:43 AM UTC
    Posted on March 30, 2011 at 09:43

    Thank you.