Skip to main content
andreasbuehler19
Associate II
Apr 26, 2005 12:15 PM UTC
Question

Simulator error: unknown mcu name

Posted on April 26, 2005 at 14:15

Simulator error: unknown mcu name

This topic has been closed for replies.

7 replies

andreasbuehler19
Associate II
Apr 13, 2005 11:21 AM UTC
Posted on April 13, 2005 at 13:21

Hello,

I want to use the simulator, just to check code, but it fails.

In [project]->[settings] I can do the mcu selection, but where

could I do the mcu configuration? Or what else do I need to

configure to get the simulator running?

Many thanks for any help.

alain2399
Visitor II
Apr 20, 2005 11:16 AM UTC
Posted on April 20, 2005 at 13:16

The mapping is defined when you go to debug mode using the blue 'D'. If it is not the first time you can change the mapping through the ''Debug instrument>Mcu configuration'' menu.

Best regards,

Alain

andreasbuehler19
Associate II
Apr 23, 2005 9:32 AM UTC
Posted on April 23, 2005 at 11:32

Hallo Alain,

many thanks for your reply. I used the blue 'D' in Debug Mode and then an error 'Simulation error: unknown mcu name' occurs.

In [Debug instruments] there is no 'Mcu Configuration' available

(I'm using ST7 Develop V3.1.1). So I don't know where to configurate

the mcu (ST72F521R6) for the debugger.

I have cnfigured the mcu in [Project]->[Settings]->[MCU Selection].

alain2399
Visitor II
Apr 25, 2005 8:21 AM UTC
Posted on April 25, 2005 at 10:21

Yes, you are right, the ST72F521AR6 and ST72F521R6 are given the error ''mcu name not supported'' when selected for the simulator. This is a bug.

The workaround is to choose the ST72521R6 or ST72521AR6 which is supported by the simulator in STVD7 r3.1.1 and there is no difference in term of simulation between this one and the F521R6 or F521AR6.

Best regards,

Alain

andreasbuehler19
Associate II
Apr 26, 2005 12:11 PM UTC
Posted on April 26, 2005 at 14:11

Hallo Alain,

that was a good idea, the simulator is working now.

Thank you!

:p

andreasbuehler19
Associate II
Apr 26, 2005 12:14 PM UTC
Posted on April 26, 2005 at 14:14

Hallo Alain,

that was a good idea, the simulator is working now.

Thank you!

:p

andreasbuehler19
Associate II
Apr 26, 2005 12:15 PM UTC
Posted on April 26, 2005 at 14:15

Hallo Alain,

that was a good idea, the simulator is working now.

Thank you!

:p