Skip to main content
ebarker
Associate II
Oct 11, 2006 12:32 PM UTC
Question

simple overflow timers

Posted on October 11, 2006 at 14:32

simple overflow timers

This topic has been closed for replies.

2 replies

stefano239955_stm1_stmicro
Associate III
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

hi,

you can use the timer as follow :

TIM_StructInit(&TIM_InitStructure);

TIM_InitStructure.TIM_Mode = TIM_PWM;

TIM_InitStructure.TIM_OC1_Modes = TIM_TIMING;

TIM_InitStructure.TIM_Clock_Source = TIM_CLK_APB;

TIM_InitStructure.TIM_Prescaler = 0x00;

TIM_InitStructure.TIM_Pulse_Length_1 = 0x0030;

TIM_InitStructure.TIM_Full_Period = 0x8000;

/* Initialize the Timer 2 */

TIM_Init(TIM3, &TIM_InitStructure);

/* Enable the Timer Overflow interrupt */

TIM_ITConfig(TIM3, TIM_IT_OC2, ENABLE);

/* Enable and configure the priority of the USB_LP IRQ Channel*/

VIC_Config(TIM3_ITLine, VIC_IRQ, 0);

to set the period....

void SetTimerPeriod(u32 per)

{

static unsigned int old_per=0;

if (old_per == per)

{

return;

}

old_per = per;

s_u32 *p = (s_u32*)&per;

if (p->h)

{

TIM_PrescalerConfig(TIM3, p->h & 0x00FF);

per /= p->h + 1;

}

else

{

TIM_PrescalerConfig(TIM3, p->h & 0x00FF);

}

TIM_SetPulse(TIM3, TIM_OC2_Channel, per);

}

static void irq_handler()

{

... your code

/*Clear the TIM OC2 flag */

TIM_ClearFlag(TIM3, TIM_FLAG_OC2);

}

ebarker
ebarkerAuthor
Associate II
May 17, 2011 7:32 AM UTC
Posted on May 17, 2011 at 09:32

Can someone show me a code fragment that will set up a timer to fire off an interrupt every 1 ms and another timer to fire off every 10 ms.

All the timers needs to is interrupt when they roll over, the isr acknowledge the interrupt, the timer reloads, and repeat......

think of it as a couple of time keepers. no external pins needed for anything,

2 timers, 1 at 1ms, 1 at 10ms, overflow reload... no-pins

Thanks,