Skip to main content
Arman Ilmak
Senior
May 10, 2018 12:43 PM UTC
Question

Simple C Question

Posted on May 10, 2018 at 14:43

Hi.

I was trying to write a code to use my keypad, but I face a problem. Because I'm new in using standard libraries I didn't face a similar problem when I was using registers(in LPC series).

#define COLUMN_PIN_1    GPIO_PIN_4

#define COLUMN_PIN_2    GPIO_PIN_5

#define COLUMN_PIN_3    GPIO_PIN_4

#define COLUMN_PIN_4    GPIO_PIN_2

#define COLUMN_PORT_1    GPIOB

#define COLUMN_PORT_2    GPIOB

#define COLUMN_PORT_3    GPIOF

#define COLUMN_PORT_4    GPIOA

for(j=1;j<5;j++)

{

if(GPIO_ReadInputPin(COLUMN_PORT_j,COLUMN_PIN_j))return (4*(i-1)+j-1);  

delay_ms(50);

}

In this code, I thought that the amount of the j will be replaced and for example when j is 1 COLUMN_PORT_j is COLUMN_PORT_1.

What should I do to achieve this purpose?

    This topic has been closed for replies.

    6 replies

    henry.dick
    Associate II
    May 10, 2018 1:04 PM UTC
    Posted on May 10, 2018 at 15:04

    The answer isn't too simple. Read a good C book if you want.

    Alternatively you can put those parameters in an array and go from there.

    See this for example.

    https://dannyelectronics.wordpress.com/2017/06/23/using-spare-output-compare-channels-as-timers-collection/

     
    Arman Ilmak
    Senior
    May 10, 2018 5:13 PM UTC
    Posted on May 10, 2018 at 17:13

    Do you know any good source for C?I searched but there are so many and I got confused which would be the best.

    Tesla DeLorean
    Guru
    May 10, 2018 5:36 PM UTC
    Posted on May 10, 2018 at 17:36

    I'd start with K&R, its a pretty much foundational text to understand what's going on and the expectations, other teaching/training books are a matter of personal style and approach to learning.

    https://en.wikipedia.org/wiki/The_C_Programming_Language

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    S.Ma
    Principal
    May 10, 2018 1:38 PM UTC
    Posted on May 10, 2018 at 15:38

    Never do this. #define is processed at compile time and is just replace a piece of text by another.

    Create a structure which contains the port and the pin position (and maybe even the result of your loop calc ?)

    Then create a const array of these, with an index you can sweep them through.

    With sizeof() you can avoid using absolute index numbers for your loop. This will take few bytes of flash...

    Tesla DeLorean
    Guru
    May 10, 2018 2:54 PM UTC
    Posted on May 10, 2018 at 16:54

    >>In this code, I thought that the amount of the j will be replaced and for example when j is 1 COLUMN_PORT_j is COLUMN_PORT_1.

    That's really not how the pre-processor works.

    ST has an example of this type of usage

    /** @defgroup STM32F4_DISCOVERY_LOW_LEVEL_Private_Variables STM32F4 DISCOVERY LOW LEVEL Private Variables

      * @{

      */

    GPIO_TypeDef* GPIO_PORT[LEDn] = {LED4_GPIO_PORT,

                                     LED3_GPIO_PORT,

                                     LED5_GPIO_PORT,

                                     LED6_GPIO_PORT};

    const uint16_t GPIO_PIN[LEDn] = {LED4_PIN,

                                     LED3_PIN,

                                     LED5_PIN,

                                     LED6_PIN};

    There are inefficient macro approaches, but these rely on the optimizer to strip the dead code paths

    /*!

     * \brief GPIOs Macro

     */

    #define RCC_GPIO_CLK_ENABLE( __GPIO_PORT__ )              \

    do {                                                    \

        switch( __GPIO_PORT__)                                \

        {                                                     \

          case GPIOA_BASE: __HAL_RCC_GPIOA_CLK_ENABLE(); break;    \

          case GPIOB_BASE: __HAL_RCC_GPIOB_CLK_ENABLE(); break;    \

          case GPIOC_BASE: __HAL_RCC_GPIOC_CLK_ENABLE(); break;    \

          case GPIOD_BASE: __HAL_RCC_GPIOD_CLK_ENABLE(); break;    \

          case GPIOH_BASE: default:  __HAL_RCC_GPIOH_CLK_ENABLE(); \

        }                                                    \

      } while(0)
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..