Skip to main content
Associate III
Oct 12, 2017 12:20 PM UTC
Question

Should we hope for long-term use of stm8?

Posted on October 12, 2017 at 14:20

Hello everybody,

Recently, the company has been actively offering to transfer your projects from 8-bit micro-controllers to 32-bit ones. In view of this, I had concerns about the feasibility of future developments with the use of STM8. I like these efficient and inexpensive processors, and I would not want to lose this engineering resource in the near future. If anyone can, anything, say about this, then please participate.

#stm8 #future
    This topic has been closed for replies.

    26 replies

    Tesla DeLorean
    Guru
    Oct 12, 2017 12:51 PM UTC
    Posted on October 12, 2017 at 14:51

    To be honest the dynamics in the semi industry have changed in recent decades, if the line remains profitable, and the fab and test equipment don't break down, or get overwhelmed by natural disaster, they are likely to continue, but when said variables turn you'll be out of luck.

    Realistically one would need to be adaptive, vastly more engineering resources and fab space are being allocated to the ARM/Cortex designs. The CM0/CM0+ being targeted at 8051 and other lower running 8-bit cores, and for compiler/tool vendors the 8-bit parts are pretty brutal targets, and least profitable.

    I'm not saying abandon any platform, just be sufficiently nibble, and prepared to port your work, and have a mindset of writing more portable code.

    Look for parts with a '10-Year Guarantee' if that's the time scale you need.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Associate III
    Oct 12, 2017 3:45 PM UTC
    Posted on October 12, 2017 at 15:45

    Many thanks for reply. You are right, we must always be prepared for the unexpected, although this and requires additional costs. I hope that this wonderful processor will take a stable place in the industry, and annoying errors in the equipment will be corrected.

    Tesla DeLorean
    Guru
    Oct 12, 2017 4:25 PM UTC
    Posted on October 12, 2017 at 16:25

    Just be mindful that decisions will be driven by accountants, not engineers and elegance of solutions.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Philipp Krause
    Senior II
    Oct 17, 2017 1:38 PM UTC
    Posted on October 17, 2017 at 15:38

    I've heard from STM8 users that ST was encouraging them to move to STM32 years ago already. On the other hand, ST is still releasing new STM8 devices (like the 8-pin devices this autumn). From the outside, it seems like there are different factions inside ST wrt. this question.

    I guess the STM8S001 being popular far beyond ST's expectations (as can be deduced from the availability at distributors after launch) might help secure a future for the STM8.

    Personally, I'd prefer if there was a second source for STM8 devices. The 8051 are still produced by many companies, even though Intel stopped making them long ago.

    On the compiler side, SDCC and related free tools are improving. For C developers, I'd expect the the STM8 toolchain situation to look quite good for a long time to come.

    Philipp

    Tesla DeLorean
    Guru
    Oct 17, 2017 4:57 PM UTC
    Posted on October 17, 2017 at 16:57

    For ST the key advantage of the STM8 is likely they don't have to pay royalties on the design, and patents on ideas/concepts other might have claim to have expired.

    Good tools don't suffer from bit-rot, the platforms they run on may lose support (DOS, Win16), I've got tools from the 1980's and 1990's I can still run and generate code just fine. I've also ported things and rebuilt DOS Extenders, and Linker/Object tools to migrate abandon-ware to run on current equipment, it's not impossible and some people can still do it. Getting support from tool vendors may be very difficult. Just be conscious that the longer you stay with a technology the more of the support/cost burden you will need to shoulder yourself.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Associate III
    Nov 8, 2017 7:11 AM UTC
    Posted on November 08, 2017 at 07:11

    Reputable Clive One,

    Tell me please, what the old high-quality compiler do you use? I also need this. And where it can be acquired?

    Pavel A.
    Oct 20, 2017 9:10 PM UTC
    Posted on October 20, 2017 at 23:10

    My 2C...  Just recently joined a new project involving a STM8L.

    They choose it only because they started from a 3rd party reference design based on that chip. Not because of cost of the chip.

    A 8-bit micro is good for one-person projects.

    With STM8, I have to roll a fragile patchwork of interrupts and 'super-loop', hard to accommodate for other developers.

    If they could use 32-bit ARM, it would be possible to bring in a decent RTOS, which is very useful to coordinate work among several developers (break functionality to 'tasks' & rich common infrastructure).

    We also consider dangers of proprietary STM8 toolchain vs what is available for ARM. The only opensource compiler there unfortunately is not supported by any GUI which is no-go for the team. (this can be done, but who has extra time? or money?)

    Back to the original question - is there still a niche for 8-bits - IMHO only a EE can answer this. 

    8-bits are low-density which means more resistant to radiation and temperature. But does this difference matter? can it be compensated by shielding?

    Power consumption of ARM M0 is not much higher than STM8 (especially 8L)  but for some applications this difference can be critical too.

    -- pa

    Philipp Krause
    Senior II
    Oct 21, 2017 11:30 AM UTC
    Posted on October 21, 2017 at 11:30

    Currently, I am not really a RTOS or IDE user. However:

    Indeed, ARM has much better RTOS availabilluty. But there are a few

    http://www.colecovision.eu/stm8/rtoses.shtml

    . Depending on your requirements they might or might not do for you. Atomthreads seems like a reasonable choice, especially due to your concerns about the toolchain situation: Atomthreads supports all 4 toolchains for the STM8 (SDCC, IAR, Cosmic, Raisonance).

    Especially in IDE support and on-target debugging, the free toolchain is not yet up to the standard of the non-free alternatives. However, it is improving rapidly. If you write portable code today using a non-free toolchain, it should be easy to change to different free or non-free toolchain later.

    There is a

    https://stm8-binutils-gdb.sourceforge.io/

    . From what I've heard on a German-language µC forum it already works quite well. SDCC 3.7.0 will have even better support for this via improved ELF/DWARF debug info output.

    The Code::Blocks IDE has support for SDCC (when I installed and started Code::Blocks a few minutes ago, it detected the installed SDCC, and gave me a choice of GCC vs. SDCC to use as the default compiler for new projects). However the SDCC support in Code::Blocks was written for older SDCC, which shows. Updating it for current SDCC seemed easy, so I

    https://sourceforge.net/p/codeblocks/tickets/567/

    . I hope it make it into the next Code::Blocks release.

    Some use SDCC with NetBeans and Anjuta, but I don't know if there is any support for SDCC in those IDEs or people are just using plain Makefiles with their projects.

    Philipp

    Associate III
    Oct 22, 2017 5:46 AM UTC
    Posted on October 22, 2017 at 05:46

    'Context-free' compiler for 'registers-free' processor it is good idea.  I would use the SDCC to build my experimental multitasking kernel, but some of its particular properties are not enabled to do this so until now. Currently, I give the advantage to COSMIC software. In view of the free license and high-quality code optimization. I think that if successful, I will make a port for the SDCC, also.

    Laurent VERA
    ST Employee
    Oct 26, 2017 3:14 PM UTC
    Posted on October 26, 2017 at 17:14

    STM8 is a product with a 

    http://www.st.com/content/st_com/en/support/resources/product-longevity.html

    from ST. We typically renew this longevity commitment at the beginning of every year. We recently introduced new 8 PIN STM8 device . STM8 volumes keep on growing, the product is very successful.
    Tesla DeLorean
    Guru
    Oct 26, 2017 5:39 PM UTC
    Posted on October 26, 2017 at 17:39

    I'm not doubting your commitment, just looking at my last 10 years in the semiconductor industry. Where your commitment will really get challenged is in year 8-9 when a 15-year old piece of critical test hardware fails and the vendor is 3 generations beyond that, no one has spare parts or the replacement runs $2M, or the vendor that encapsulates the package goes bankrupt or merges with a competitor, or the factory gets destroyed in an earthquake/tsunami or is in the middle of a radioactive no go zone.

    These things are ultimately predicated by business conditions.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Laurent VERA
    ST Employee
    Oct 26, 2017 5:58 PM UTC
    Posted on October 26, 2017 at 17:58

    Hi Clive,

    Actually, all this is a matter of supply chain management and business continuity plan.

    In the semiconductor business, volume is key to maintain production.

    If you were to sell a custom product for a very high volume application (such as a mobile phone for instance), it would be difficult to commit on a 10 year production since your volume rely on a single product / single application. 

    STM8 and STM32 are used in thousands of end products, we do not rely on a major customers to drive our volumes. We know volumes will not drop in the next 10 years. The vast majority of our customers have extremly long design cycles.

    For the production facilities, we have a dual sourcing policy either running or as a back up (wafer diffusion / test / assembly).