Skip to main content
jrichards
Visitor II
Jul 17, 2011 7:55 PM UTC
Question

Setting RTC wake up timer for perioic wake up

Posted on July 17, 2011 at 21:55

I've pored over the user guide and various app notes but cannot seem to get the RTC wakeup timer to start running, so no WU interrupt and I get stuck in halt mode.

Can someone give me a difinitive checklist of what register bits need to be set/reset to get the timer started. I need to check that what I think I should be doing from reading the user manual is right.

Many thanks

Jeremy

    This topic has been closed for replies.

    3 replies

    Stm32User
    Associate III
    Jul 29, 2011 10:49 AM UTC
    Posted on July 29, 2011 at 12:49

    I am using STM8L151 with external 32khz crystal ( LSE)

    Here is the setup code, in my application used as a 50ms systick interrupt

     CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE);

     CLK_RTCClockConfig(CLK_RTCCLKSource_LSE, CLK_RTCCLKDiv_1);

     RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div16);

     RTC_ITConfig(RTC_IT_WUT, ENABLE);

     

    RTC_SetWakeUpCounter(_50ms_TIMER_VAL);

     RTC_WakeUpCmd(ENABLE);

    then enable interrupts 

    RTC_ITConfig(RTC_IT_WUT, ENABLE);

    In interrupt handler clear the interrupt source 

    if( RTC_GetFlagStatus(RTC_FLAG_WUTF) == SET )

    {

       RTC_ClearITPendingBit(RTC_IT_WUT);

    }

    hakan23
    Associate
    Jan 15, 2013 1:57 PM UTC
    Posted on January 15, 2013 at 14:57

    Hello Patrick

    Are you still working with this processor ??

    Can you please send the smallest possible complete example for this ??

    best regards

      Hakan

    Stm32User
    Associate III
    Jan 24, 2013 7:03 PM UTC
    Posted on January 24, 2013 at 20:03

    I would use the firmware library as its already written,tested and documented. You can then spend time on your application instead of wasting time re-writing something which already works. 

    You can download the firmware library here:-

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/stm8l15x_stdperiph_lib.zip

    If you really want to minimise the code size then for each of the function calls in the code strip out the lines of code you need.

    For example 

     CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE);

    Find this function, look at the code and strip out the lines of code which actually enable the peripheral.