Skip to main content
wdcai
Associate III
October 15, 2004
Question

Second uart

Posted on October 15, 2004 at 04:56

Second uart

This topic has been closed for replies.

3 replies

lwang
Associate II
May 17, 2011
Posted on May 17, 2011 at 12:03

Whenever the address of a SFR is divisible by 8, that SFR is bit addressable!

joseph2399
Associate II
May 17, 2011
Posted on May 17, 2011 at 12:03

The second UART in the uPSD33xx devices is bit addressable. The second UART in the uPSD32xx devices is only byte addressable. I am not sure what demo code you are looking at, but it is probably a carryover from the 32xx and was not updated to take advantage of the bit addressability available in the 33xx.

wdcai
wdcaiAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 12:03

Hi,All!

Can some SFR about second uart ,such like scon2, be read or written in bit mode? The demo source code provided by ST operates this SFR in BYTE mode!

Thanks!