Skip to main content
Philipp Krause
Senior II
Jun 11, 2015 4:18 PM UTC
Question

sdcc 3.5.0 rc1

Posted on June 11, 2015 at 18:18

sdcc 3.5.0 is to be released soon. There already is release candidate 1.

You can download the release candidate and have a look at it. The more eyes on it, the less likely are hidden bugs.

The main changes from previous sdcc 3.4.0 are:

* Many fixes and improvements in the stm8 port

* --disable-non-free configure option

* z80 port fixes

* long long fixes

* Changed default language dialect from --std-sdcc89 to --std-sdcc99

* Reorganized and updated manual

* Reduced memory consumption (most noticeable for high --max-allocs-per-node)

* Faster compilation for stm8 (most noticeable for high --max-allocs-per-node)

* atoll() function for conversion of strings to long long

* __z88dk_fastcall and __z88dk_callee calling conventions for more efficient function calls and better compability with z88dk

* --lospre-unsafe-read renamed to --allow-unsafe-read

Due to the substantial improvements, in particular in the stm8 port, I think all STM8 programmers will want to change from 3.4.0 to 3.5.0.

Philipp

    This topic has been closed for replies.

    2 replies

    jagspaul
    Associate
    Jun 13, 2015 5:55 PM UTC
    Posted on June 13, 2015 at 19:55

    I am using SDCC 3.50 for STM8.

    I ma getting compiling error while using code/near/__data/eeprom.

    ex.

    __code uint8_t test_char

    [2]

    = {{1},{2}};

    Can you help me how to use following options

    data

     

    near

    far

     

    code

    regards

    jags

    Philipp Krause
    Senior II
    Jun 13, 2015 9:02 PM UTC
    Posted on June 13, 2015 at 23:02

    These keywords are not part of the C standard, but compiler extensions supported for some backends by sdcc. They are currently not supported for stm8. __data and __code are not planned to be implemented, as they are not useful on stm8. __near and __far will proably be implemented in the future, but they are not as important on stm8 as on other architectures, as they only provide a small benefit on stm8.

    Philipp