Skip to main content
celine2
Associate II
Aug 28, 2006 5:41 AM UTC
Question

SCI 57600 bauds is it possible?

Posted on August 28, 2006 at 07:41

SCI 57600 bauds is it possible?

This topic has been closed for replies.

2 replies

celine2
celine2Author
Associate II
Aug 25, 2006 11:57 AM UTC
Posted on August 25, 2006 at 13:57

Hi,

Is it possible to transmit informaion on SCI ports with a bauds rate equals to 57600 or not?

I have ST72334 with a quartz (8MHz).It doesn't work.

But with a quarz 16MHz, is it possible to communicate?

SCIETPR=0x09; => 55 555 bauds

So, the mistake is 3.5%.

Is it good or not ?

thank you.

[ This message was edited by: Philippe13 on 25-08-2006 17:41 ]

wolfgang2399
Associate III
Aug 28, 2006 5:41 AM UTC
Posted on August 28, 2006 at 07:41

Hi Philippe,

with standard transmitter it should work. Although I didn't find anything about the required accuracy I remember an allowed tolerance of 5%.

But also consider the maximum cable-length. From my experience it should not exceed 1.5m with a baud-rate of 57,6kbauds.

By the way: I prefer to use a crystal of 7.3728MHz or even 3.6864MHz wich both are usual standards. You can reach baud-rates up to 115.2kbps with the 3,6864MHz crystal.

The only little inconvenience resulting from this solution: You must calculate all the timings depending on this frequency.

Best regards

WoRo