Skip to main content
khaled
Associate
Mar 9, 2007 1:41 PM UTC
Question

saving video in SMI

Posted on March 09, 2007 at 14:41

saving video in SMI

This topic has been closed for replies.

2 replies

khaled
khaledAuthor
Associate
Mar 6, 2007 12:17 PM UTC
Posted on March 06, 2007 at 13:17

Hi,

I am a student (don’t forget).

I am working on the STR750-EVAL.

I want to receve picture(or video) on the UART0 and save it in the SMI.

I want to accelerate registering in the flash so I will use 2 buffers :1 to write into from the UART and at the same time copy the second buffer into SMI.

So how can use SMI to do like this?

Is it possible to use DMA?

kaouther
Associate II
Mar 9, 2007 1:41 PM UTC
Posted on March 09, 2007 at 14:41

Hello,

you could use the STR750 application note used for internal flash*

to load the image to the internal

You could use the IAP driver which allows to download a binary file via HyperTerminal to the STR75x internal Flash. Then you could modify to load your image in the SPI memory instead of the internal flash and use the DMA.

The application note is available on the web site.

Hope it helps.