Skip to main content
bernard2399
Associate
Mar 31, 2006 4:56 AM UTC
Question

RTC and STOP MODE

Posted on March 31, 2006 at 06:56

RTC and STOP MODE

This topic has been closed for replies.

4 replies

bernard2399
Associate
Mar 21, 2006 6:37 PM UTC
Posted on March 21, 2006 at 19:37

Hi.

Can the RTC kicks back the STR710 to life when it is in stop mode? The datasheet is not explicit about that.

Thanks!

Bernard

hichem2
Associate
Mar 23, 2006 4:43 AM UTC
Posted on March 23, 2006 at 05:43

Hi,

The device can be Wake-up from STOP mode by the configured external wake-up lines (XTI unit), and the RTC alarm can be mapped as External Interrupt Line (line 15).

By the way, the RTC can kicks back the STR710 to life when it is in stop mode. :p :D

regards,

Hich

shangshuai
Associate
Mar 31, 2006 3:04 AM UTC
Posted on March 31, 2006 at 05:04

Hi,

Can rtc still work with vdd33 off and v18back on?

thanks

hichem2
Associate
Mar 31, 2006 4:56 AM UTC
Posted on March 31, 2006 at 06:56

Hello,

For the RTC operation you will have to keep the 3.3V supply on the V33 pins.

Only in Standby mode keeping V3.3, in order to reduce power consumption it is possible to bypass the Low Power Voltage regulator but V18BKP pin must be connected to an external 1.8V through a diode in this case.

Hope that this can helps,

REgards,

Hich :-]