Skip to main content
Visitor II
October 30, 2024
Question

Routing for USBLC6-2SC6

Hi,

I am creating my own PCB based on the Nucleo144pin board. From what I understand, the USBLC6-2SC6 is meant to be an ESD protection IC. The USBLC6-2 datasheet recommends that the input is not connected to the output. However, the inputs from the USB connector is shorted to the output of the USBLC6-2SC6 in the Nucleo144pin board. Is there an intended function for this or is it an error?

75a81f4f-f72b-4335-8098-f16a96d3363e.jpg53e3ca53-5fab-4347-b044-2142647b0fc9.jpgPCB.JPG

This topic has been closed for replies.

1 reply

Associate
May 20, 2025

Hi! the routing between terminals allow to not mount the USBLC6 on the nucleo board. As you say, this is not recommended for optimum protection.