Skip to main content
spiovan9
Associate III
Oct 10, 2011 7:47 PM UTC
Question

Rotary potentiometer code

Posted on October 10, 2011 at 21:47

Hi all,

some piece of code to manage a rotary encoder potentiometer. The model I use is from the chinese market maybe by TREXON. I'll propose both interrupt and polling mode. The interrupt code has been adapted from http://www.arduino.cc/playground/Main/RotaryEncoders and the polling one from http://stackoverflow.com/questions/34735/using-a-rotary-encoder-with-avr-micro-controller. Find also the interrupt handler (just modify the stm8s_it.c code as indicated).

The code is a part of a hobby project which is a PLL 2.4GHz signal reference generator.

The rotary potentiometer if for making a ''knob'' for such a generator to move the output frequency of the PLL. The project also has a 12 keys keypad and a LCD 16x2 display, which I have already posted.

The rotary potentiometer CHA goes into GPIOB.PIN0 and the CHB into the GPIOB.PIN1.

Hope it helps.

Stefano

________________________

main()

{

..

..

while(1)

    {

        

&sharpifdef _POLLMODE_

        wheel = (GPIO_ReadInputData(GPIOB) & 0x03);

        if(dir == 0)

        {

            if(wheel == 0x01)

                dir = 2;

            else if (wheel == 0x02)

                dir = 4;

            else

                dir = 0;

        }

        else if (dir == 2)

        {

            if (wheel == 0x01)

                dir = 2;

            else if (wheel == 0x00)

            {

                // decrease frequency

                VCOFreq -=100;

                PLL_SetFreq(VCOFreq);

                LCD_Cmd(LINE_2);

                Int2Str(sz_Val, VCOFreq);

                pos = 7;

                LCD_Str(sz_Val);

                dir = 0;

            }

            else

                dir = 0;

        }

        else if (dir == 4)

        {

            if (wheel == 0x02)

                dir = 4;

            else if (wheel == 0x00)

            {

                // increase frequency

                VCOFreq +=100;

                PLL_SetFreq(VCOFreq);

                LCD_Cmd(LINE_2);

                Int2Str(sz_Val, VCOFreq);

                pos = 7;

                LCD_Str(sz_Val);

                dir = 0;

            }

            else

                dir = 0;

        }

        else if (wheel == 0x03)

        {

            dir = 0;

        }

&sharpelse // INT MODE

    if (changed)

        {

            BEEP_Cmd(ENABLE);

            VCOFreq = counter;

            PLL_SetFreq(VCOFreq);

            LCD_Cmd(LINE_2);

            Int2Str(sz_Val, VCOFreq);

            pos = 7; // force cursor position <> 0 to simulate typing a new value from the keyboard

            LCD_Str(sz_Val);

            changed = 0;

            BEEP_Cmd(DISABLE);

        }

&sharpendif

____________________

/**

  * @brief External Interrupt PORTB Interruption routine.

  * @par Parameters:

  * None

  * @retval

  * None

*/

&sharpifdef _COSMIC_

@far @interrupt void EXTI_PORTB_IRQHandler(void)

&sharpelse /* _RAISONANCE_ */

void EXTI_PORTB_IRQHandler(void) interrupt 4

&sharpendif /* _COSMIC_ */

{    

    u8 portval;

    

    portval = (GPIO_ReadInputData(GPIOB) & 0x03);

    if ((portval == 0x03) || (portval == 0x00))

    {

        counter-=200;

    }

    else

    {

        counter+=200;

    }

    changed = 1; // this is to tell the main to display the new value

    

}

#interrupt #encoder
This topic has been closed for replies.