Skip to main content
This topic has been closed for replies.

6 replies

e239955_stm1_stmicro_com
Associate III
Aug 4, 2005 1:12 PM UTC
Posted on August 04, 2005 at 15:12

Hello,

Does anybody know the reset value of:

- PC0

- PC1

- PC2

- PD

THX

Manu

boris239955
Associate II
Aug 5, 2005 5:57 AM UTC
Posted on August 05, 2005 at 07:57

Port 0 :

PC0 = 0xffff

PC1 = 0xffff

PC2 = 0x0

PD = 0xe0ff

Port 1 :

PC0 = 0xffff

PC1 = 0xffff

PC2 = 0x0

PD = 0xfcff

Port 2 :

PC0 = 0xffff

PC1 = 0xffff

PC2 = 0x1

PD = 0xff0f

These are the values that can be derived from the Reference Manual, if I'm understanding it correctly.

(On my STR711, however, it seems that P0.15 is configured for TTL input at reset. This is not mentionned in the docs.)

Can anybody at ST confirm the values ?

e239955_stm1_stmicro_com
Associate III
Aug 5, 2005 6:05 AM UTC
Posted on August 05, 2005 at 08:05

Thank you,

where did you find the reset value in the reference manual ?

(I didn't find it, there's just an asterisk)

boris239955
Associate II
Aug 5, 2005 7:10 AM UTC
Posted on August 05, 2005 at 09:10

The values are not explicitely written in the Reference Manual, but you can calculate them using the information in the Device Pin Description table (see page 22).

e239955_stm1_stmicro_com
Associate III
Aug 5, 2005 7:19 AM UTC
Posted on August 05, 2005 at 09:19

OK, thanks

ongth60
Associate III
Oct 28, 2005 3:02 AM UTC
Posted on October 28, 2005 at 05:02

Hi,

Can someone confirm the pin configurations upon reset here?

Rgrds,

ongth60