Skip to main content
fcasa.16
Associate II
April 7, 2021
Question

Reset forced low

Hi,

while the software are working, suddenly it will become stop, and reset pin is permanently forced low, it freaks me out!! Someone will help me, thank you so mutch

    This topic has been closed for replies.

    10 replies

    Javier1
    Principal
    April 7, 2021

    what do you mean with permanently?

    hit me up in https://www.linkedin.com/in/javiermuñoz/
    fcasa.16
    fcasa.16Author
    Associate II
    April 7, 2021

    Thank you Javier

    reset pin goes to 0 Volt and doesn't work until the power is off. It seems to be frozen.

    this appens especially when we are getting strong electric interference

    fcasa.16
    fcasa.16Author
    Associate II
    April 7, 2021

    Thank you Javier

    reset pin goes to 0 Volt and doesn't work until the power is off. It seems to be frozen.

    this appens especially when we are getting strong electric interference

    Javier1
    Principal
    April 7, 2021

    @fcasa.16​ maybe show us some pictures/schematics or explain a little bit more your issue.

    hit me up in https://www.linkedin.com/in/javiermuñoz/
    WilkoL
    Senior
    April 7, 2021

    And the GPIO next to the RESET pin?

    Also, what chip do you use? On some you can change the RESET pin into PA1.

    fcasa.16
    fcasa.16Author
    Associate II
    April 8, 2021

    MCU: STM8L151C8T6 , below section of schematic, RESET, after power on, change in PA1 Output OD and SWIM change in PA0. I'm at my wits end

    WilkoL
    Senior
    April 8, 2021

    Is it possible to NOT re-use RESET and SWIM? Because my guess is that your problem has something to do with that. I never use those pins for anything else than programming and debugging. If I need more pins than available I upgrade to a bigger microcontroller.

    So (if possible) see if the problem still happens when you don't do anything with PA0 and PA1.

    fcasa.16
    fcasa.16Author
    Associate II
    April 8, 2021

    Unfortunately, problem still happen even if I not reuse reset and swim.

    WilkoL
    Senior
    April 8, 2021

    Without having the pcb and code here it is hard to guess. It can be all sorts of things, floating GPIO doing strange things, a short between another pin and the RESET line, an error in the code causing the RESET to be pulled low...

    Single stepping through the code isn't possible I think, because you said the microcontroller will work for a while, you might be single stepping for ages. Maybe logging things, for example by sending data out via a uart and recording it with Notepad++ will give you some clues.

    fcasa.16
    fcasa.16Author
    Associate II
    April 8, 2021

    I'm not really sure, but issue could be a failure about internal BOAT LOADER. I did detect defect only on those with the same serial number

    Thank you for your assistance.